Question
uart baud rate supported by internal 48Mhz oscillator
Posted on July 29, 2016 at 04:52
I am using this STM32F0 MCU
http://www.st.com/content/ccc/resource/technical/document/datasheet/0a/d2/ad/ae/d4/04/44/e3/DM00098745.pdf/files/DM00098745.pdf/jcr:content/translations/en.DM00098745.pdfIt has an internal 48Mhz oscillator. I am thinking of saving material cost by using this internal 48Mhz oscillator and not use an external crystal but I am worried that the uart will not be accurate. I only need to use a baud rate of up to 38.4kbps. Is this internal 48Mhz oscillator good enough for 38.4kbps baud rate?Another question is what if I am going to use multiple uarts, say up to 4 uarts. Does the accuracy of the oscillator matter in this case? Is it the same whether 1 uart is used or all 4 uarts are going to be used?