Skip to main content
ezrab
Associate III
Oct 6, 2010 1:35 PM UTC
Question

Uart application

Posted on October 06, 2010 at 15:35

hi

i was tring to activate USART3 On Port C PC10,PC11.

 

i used this configuration :

USART3->CR1 = 0x0C; //Receiver enable, Transmitter enable, USART disable

    USART3->CR2 = 0x0;

    USART3->BRR=156;//9600 at 24Mhz

   setsystemclock(); //set system clock to 24Mhz

 

    AFIO->MAPR|=0x10;//port remap as uart //PC10 TX PC11 RX

    GPIOC->CRH=0x4B00; //PC11 in input floating mode for RX. PC10 Alternative Output TX.

    RCC->APB2ENR |=0x40000;

 USART3->CR1 |=2000; //Uart Enable;

  while(1)

  {

   while(TxCounter < 30)

  {

    /* Send one byte from USARTy to USARTz */

      USART3->DR =( TxBuffer[TxCounter] & (uint16_t)0x01FF);

      while(((USART3->SR)&0x40)>0);//wait transmition complete

    TxCounter++;

    /* Loop until USARTy DR register is empty */

  }

  TxCounter=0;

  //GPIOC->ODR=0x3ffff;

  //GPIOC->ODR=0x0;

  }

but for some reason  it does not work??

can you help?

thanks.
    This topic has been closed for replies.

    15 replies

    ezrab
    ezrabAuthor
    Associate III
    Oct 11, 2010 7:06 AM UTC
    Posted on October 11, 2010 at 09:06

    hi.

    thanks for all your help.

    i have another question.

    how did you get to the number 0x9c4?

    what is the math behind it?

    thanks.

    Tesla DeLorean
    Guru
    Oct 11, 2010 2:46 PM UTC
    Posted on October 11, 2010 at 16:46

    how did you get to the number 0x9c4?

    24,000,000 / 9,600 = 2,500 = 0x9C4

    This uses the fact that while the USART is using a 1/16th clock it also represents the baud rate divider with a 4-bit fixed point fractional component.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    stephenflowers9
    Visitor II
    Oct 22, 2010 8:08 AM UTC
    Posted on October 22, 2010 at 10:08

    I also had problems getting USART2 working.  I followed the guidance on this thread and solved the problem but cant help feel I am missing some documentation where it implicitly says to enable the clocks first? I`m new to ARM processors but not to programming

    joa
    Visitor II
    Oct 22, 2010 8:36 AM UTC
    Posted on October 22, 2010 at 10:36

    From ''RM0041 Reference Manual'' for stm32f100xx, last paragraph in section 2.1:

    After each device reset, all peripheral clocks are disabled (except for the SRAM and FLITF).

     

    Before using a peripheral you have to enable its clock in the RCC_AHBENR,

     

    RCC_APB2ENR or RCC_APB1ENR register.

     

    Tesla DeLorean
    Guru
    Oct 22, 2010 12:47 PM UTC
    Posted on October 22, 2010 at 14:47

    I also had problems getting USART2 working.  I followed the guidance on this thread and solved the problem but cant help feel I am missing some documentation where it implicitly says to enable the clocks first? I`m new to ARM processors but not to programming

     

    It is a synchronous part, unless the parts are clocked they are non-functional and non-responsive. CMOS parts draw the majority of their current when signals transition, if you turn off clocks it will consume less power, unused peripherals are turned off to save power.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..