Skip to main content
Visitor II
September 13, 2024
Question

U585 coming up from shutdown every +-30 seconds, when I'm trying to configure for every 5 mins

Hi.

I'm trying to configure a wake-up alarm (Alarm A) to wake up (for a test) after 5 minutes, being time 0 when I turn it on, but I can't even make it work the first alarm because it keeps waking up every 30 seconds or so.

I'm using the U585.

Sometimes the alarm A flag becomes 1, and it works, but it's rare.

Here is the code related to that:

int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */
 __HAL_DBGMCU_FREEZE_IWDG();
 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* Configure the System Power */
 SystemPower_Config();

 /* USER CODE BEGIN SysInit */

 wakeup_reason = get_wakeup_reason();
 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_DCACHE1_Init();
 MX_ICACHE_Init();
 MX_USART1_UART_Init();
 MX_IWDG_Init();
 MX_TIM5_Init();
 MX_RTC_Init();
 MX_I2C2_Init();
 MX_ADC1_Init();
 MX_SPI1_Init();
 MX_TIM1_Init();
 MX_SAI1_Init();
 MX_TIM7_Init();
 MX_TIM15_Init();
 MX_TIM16_Init();
 /* USER CODE BEGIN 2 */
 __HAL_RCC_PWR_CLK_ENABLE(); // I don't know if this should be here, elsewhere or even not called

 if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) != RESET)
 {
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF);

 if (__HAL_RTC_ALARM_GET_FLAG(&hrtc, RTC_FLAG_ALRAF) != RESET)
 {
 flagWakeUpScheduling = true;

 __HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF);
 }
 }
 custom_main();
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 }
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
uint8_t get_wakeup_reason()
{
 if (__HAL_RCC_GET_FLAG(RCC_FLAG_BORRST))
 {
 __HAL_RCC_CLEAR_RESET_FLAGS();
 }
 if (__HAL_PWR_GET_FLAG(PWR_WAKEUP_FLAG1) ||
 __HAL_PWR_GET_FLAG(PWR_WAKEUP_FLAG7))
 {
 __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG1);
 __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG7);
 }
 MX_GPIO_Init();
 GPIO_InitTypeDef GPIO_InitStruct = { 0 };

 // enter_sleep(); // commented here so the other wake ups won't make it sleep again
 return 0;
}
/* RTC init function */
void MX_RTC_Init(void)
{
 /* USER CODE BEGIN RTC_Init 0 */

 /* USER CODE END RTC_Init 0 */

 RTC_PrivilegeStateTypeDef privilegeState = {0};
 RTC_TimeTypeDef sTime = {0};
 RTC_DateTypeDef sDate = {0};
 RTC_AlarmTypeDef sAlarm = {0};

 /* USER CODE BEGIN RTC_Init 1 */

 /* USER CODE END RTC_Init 1 */

 /** Initialize RTC Only
 */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 127;
 hrtc.Init.SynchPrediv = 255;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
 hrtc.Init.BinMode = RTC_BINARY_NONE;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
 privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO;
 privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE;
 privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0;
 privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0;
 if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK)
 {
 Error_Handler();
 }

 /* USER CODE BEGIN Check_RTC_BKUP */
 // UNUSED(sTime);
 // UNUSED(sDate);
 // UNUSED(sAlarm);

 /* USER CODE END Check_RTC_BKUP */

 /** Initialize RTC and set the Time and Date
 */

 sTime.Hours = 0;
 sTime.Minutes = 0;
 sTime.Seconds = 0;
 sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
 sTime.StoreOperation = RTC_STOREOPERATION_RESET;
 if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
 {
 Error_Handler();
 }
 sDate.WeekDay = RTC_WEEKDAY_MONDAY;
 sDate.Month = RTC_MONTH_JANUARY;
 sDate.Date = 1;
 sDate.Year = 0;
 if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable the Alarm A
 */
 sAlarm.AlarmTime.Hours = 0;
 sAlarm.AlarmTime.Minutes = 5;
 sAlarm.AlarmTime.Seconds = 0;
 sAlarm.AlarmTime.SubSeconds = 0;
 sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
 sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL;
 sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
 sAlarm.AlarmDateWeekDay = 1;
 sAlarm.Alarm = RTC_ALARM_A;
 if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BIN) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable the Alarm B
 *//*
 sAlarm.Alarm = RTC_ALARM_B;
 if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BIN) != HAL_OK)
 {
 Error_Handler();
 }
 */
 // Enable the WakeUp
 // I'm not sure if this next line should be commented or not; both ways don't work
 if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* USER CODE BEGIN RTC_Init 2 */

 /* USER CODE END RTC_Init 2 */

}
void custom_main(void)
{
 // HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1); // is this needed?

 HAL_PWR_EnableBkUpAccess();
 DWT_Delay_Init();

 // WatchDog Refresh
 HAL_IWDG_Refresh(&hiwdg);

 while (1)
 {
	 if (__HAL_RTC_ALARM_GET_FLAG(&hrtc, RTC_FLAG_ALRAF) != RESET)
	 {
	 flagWakeUpScheduling = true; // it never gets to here

	 __HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF);
	 }
	 if (flagWakeUpScheduling)
	 {
	 	flagWakeUpScheduling = false;
 }
}

 I know I have a part that is repeated twice, but knowing that *sometimes* the RTC_FLAG_ALRAF is true, I tried catching it in other moments.

Thanks in advance.

This topic has been closed for replies.