Skip to main content
gfuehrer
Associate III
June 5, 2013
Question

Typos in Reference Manuals for STM32F3

  • June 5, 2013
  • 5 replies
  • 919 views
Posted on June 05, 2013 at 22:36

  told me to report on this forum any corrections needed in reference docs and code.

These corrections apply to the latest published reference manuals for STM32F3xx:

RM0316: STM32F302xx, STM32F303xx and STM32F313xx advanced ARM-based 32-bit MCUs DM00043574.pdf

DocID 022558 Rev 2.0

RM0313: STM32F37xx and STM32F38xx advanced ARM-based 32-bit MCUs DM00041563.pdf

DocID 022448 Rev 1.0

1) Table 24. Programmable data width & endian behavior; Source port width=32, Destination port width=16: Transfer operations should read ''WRITE BxBy[15:0]'' not ''...[7:0]''

2) USART Section 5.4 Baud rate generation; Example 1 In case of oversampling by 8: calculation should read ''0x3 >> 1'' not ''... << 1''.

-Gary

#corrections-reference-manual #corrections-reference-manual
    This topic has been closed for replies.

    5 replies

    Amel NASRI
    ST Technical Moderator
    June 6, 2013
    Posted on June 06, 2013 at 11:40

    Hello Gary,

    Thanks for your contribution.

    We will try to implement your feedbacks in coming versions.

    Best Regards,

    ST.MCU

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    gfuehrer
    gfuehrerAuthor
    Associate III
    June 6, 2013
    Posted on June 06, 2013 at 23:34

    Here are a few more.

    RM0316: STM32F302xx, STM32F303xx and STM32F313xx advanced ARM-based 32-bit MCUs DM00043574.pdf

    DocID 022558 Rev 2.0

    1) GPIO Section 4.3 (and in Table 22) GPIOx_OSPEEDR Reset value for Port A: Should be ''0x0C000000'' not ''0x64000000''.

    2) GPIO Section 4.4 (and in Table 22) GPIOx_PUPDR Reset value for ports C-F: Should be ''0x00000000'' not ''0x0C000000''.

    RM0313: STM32F37xx and STM32F38xx advanced ARM-based 32-bit MCUs DM00041563.pdf

    DocID 022448 Rev 1.0

    1) GPIO Section 4.1 (and in Table 22) GPIOx_MODER Reset value for Port A: Should be ''0xA8000000'' not ''0x28000000''. Reset value for Port B: Should be ''0x00000280'' not ''0x00000000''.

    2) GPIO Section 4.3 (and in Table 22) GPIOx_OSPEEDR Reset value for Port A: Should be ''0x0C000000'' not ''0x00000000''. Reset value for Port B: Should be ''0x000000C0'' not ''0x00000000''.

    3) GPIO Section 4.4 (and in Table 22) GPIOx_PUPDR Reset value for ports A: Should be ''0x64000000'' not ''0x24000000''. Reset value for ports B: Should be ''0x00000100'' not ''0x00000000''.

    -Gary
    Amel NASRI
    ST Technical Moderator
    June 13, 2013
    Posted on June 13, 2013 at 10:50

    Hello Gary,

    Will check for RM0313 but I don't understand how did you get new reset values that you suggest for RM0316.

    Could you please explain?

    Thanks & Regards,

    ST.MCU

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    gfuehrer
    gfuehrerAuthor
    Associate III
    June 13, 2013
    Posted on June 14, 2013 at 01:42

    I loaded the following for firmwareusing the STM32 ST-LINK Utility:

    void __attribute__((noreturn)) Reset_Handler() 
    { 
    // Need to enable the port clocks 
    RCC->AHBENR |= RCC_AHBENR_GPIOAEN|...|RCC_AHBENR_GPIOEEN; 
    for (;;) { } 
    } 

    Then I examined the register values in the Device Memory window. -Gary
    Amel NASRI
    ST Technical Moderator
    June 19, 2013
    Posted on June 19, 2013 at 16:13

    Hello Gary,

    You are right.

    Thanks again for your contribution. Your feedbacks will be taken into account in next reference manuals releases.

    Mayla

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.