Skip to main content
Associate II
Apr 12, 2024 7:37 AM UTC
Question

Typical pull-up resistance value

Hi,

 

Greetings @Peter BENSCH 

 

I am using STM32G431MB controller in my project. I am configuring PB4 as my General purpose Input pin. Ports PB5-PB9 as well as PC8,PC9, PA8 and PA9 are assigned as General purpose outputs connected to Analog HART Mux. In the datasheet, the recommended pull up values are minimum:25K; Typical 40K and Maximum 60K for I/O pins.

 

Can you kindly suggest if we could use minimum value of 25K as pull up resistors for the pins.

 

Regards<
Sreejith

This topic has been closed for replies.

3 replies

waclawek.jan
Super User
Apr 12, 2024 8:37 AM UTC

That's value of the internal pullup, and *not* some recommended external pullup.

Whether its value (taking into account the spread given by technology) is adequate for your application, is up to you to judge.

JW

 

Danish1
Lead III
Apr 12, 2024 8:41 AM UTC

I think you misunderstand the data-sheet.

Those are not "recommended" pull-up values. That is the effective resistance of built-in pull-up resistors, which you can choose to turn on (or not) when the pin is programmed as digital-input or open-drain-output.

There are circumstances where you might choose to have your own external pull-up resistors. These include ensuring the pin is in a certain state even when the stm32 is reset or in its lowest-power shutdown. Or if the value of the built-in pull-up is not appropriate for your application. (You could want a lower value if you need a certain minimum current to maintain healthy switch contacts or better noise-immunity, or a higher value if you wish to have lower current drain when the pin is driven low externally).

Billy OWEN
ST Employee
Apr 12, 2024 2:00 PM UTC

Hi @sreejithrnair 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy