Skip to main content
Associate
November 27, 2025
Question

Type III Format Interface Descriptor

Hi everyone!

I figure out that Type III Format Interface Descriptor is generated automatically on STM32L476RG, and this use encoder format to transmit audio (Not PCM). Frame size vary an do mot match PCM packet sizes, meaning that transmitting  raw PCM using Format Type III result as no audio output.

However, apparently those problems doesn't occur using Format |Type I Interface descriptor.

Any idea  about how can to solve this problem? 

Thanks.

1 reply

mƎALLEm
ST Technical Moderator
December 1, 2025

Hello,


@jimmyibongo wrote:

I figure out that Type III Format Interface Descriptor is generated automatically on STM32L476RG


Generated by what?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.