Skip to main content
Associate II
June 11, 2024
Solved

Tying SPI inputs together to run several ADCs at once

Dear Community,

I'm working on STM32H743ZIT6 based project.

Here I want to set up 4 ADCs which have SPI interface.

On developer's forum is said "If all ADCs will be sampled at the same point in time with the same settings, then the SCLK, CS, and SDI can be tied together".

Also there mentioned: "Make sure the digital interface is able to drive all of the ADCs at once".

Is STM32H743ZIT6 able to drive all of the ADCs at once?

According to electrical characteristics:

Digital high input voltage logic level - 0.7V x DVDD (min) / DVDD + 0.3V (max);

Digital low input voltage logic level - -0.3 (min) / 0.2 x DVDD (max).

DVDD = 3.3V

 

Thanks!

This topic has been closed for replies.
Michal Dudka
Michal DudkaBest answer
Lead
June 12, 2024

You need to route:
SCK from first SPI master to all ADCs and all SPI slaves
MOSI from first SPI master to all ADCs SDI
SDO from ADC1 to MISO of SPI master 
SDO from ADC2 to MOSI of first SPI slave 
SDO from ADC3 to MOSI of second SPI slave
SDO from ADC4 to MOSI of third SPI slave
CS from STM32 to all ADCs

18 replies

AScha.3
Super User
June 11, 2024

Hi,

>Is STM32H743ZIT6 able to drive all of the ADCs at once?

Which ADC ? + SPI clk at ... ?

+

And where going the 4 SDO with data to ?

 

If you feel a post has answered your question, please click on " Best Answer ".
Michal Dudka
Lead
June 11, 2024

It is OK to drive multiple ADS8685 by one set of SCK/SDI/CS lines... but what is your question ?