Skip to main content
parisa
Associate III
Mar 1, 2017 2:27 PM UTC
Solved

two USART configuration failed (USART3 problem)

Posted on March 01, 2017 at 15:27

Hi,

Here is my code for configuring two different usart but my USART3 doesn't work properly and USART2 works fine.(I remap both of them). what is my mistake that I didn't pay attention?

Problem: I don't have any signal on USART3_TX pin when I send a char. however my USART1 works fine(send and receive)

    USART_InitTypeDef USARTConfiguration;

    GPIO_InitTypeDef GPIOS;

        RCC_APB2PeriphClockCmd(RCC_APB1Periph_USART2|RCC_APB1Periph_USART3|RCC_APB2Periph_GPIOD |RCC_APB2Periph_GPIOC |RCC_APB2Periph_AFIO,ENABLE);

 GPIO_PinRemapConfig(GPIO_Remap_USART2|GPIO_PartialRemap_USART3,ENABLE);

    

    GPIOS.GPIO_Mode=GPIO_Mode_AF_PP ;

    GPIOS.GPIO_Speed=GPIO_Speed_50MHz;

    GPIOS.GPIO_Pin=GPIO_Pin_5;

    GPIO_Init(GPIOD,&GPIOS);

    

    GPIOS.GPIO_Mode=GPIO_Mode_IN_FLOATING ;

    GPIOS.GPIO_Pin=GPIO_Pin_6;

    GPIO_Init(GPIOD,&GPIOS);

               

    USARTConfiguration.USART_BaudRate=9600;

    USARTConfiguration.USART_StopBits=USART_StopBits_1;

    USARTConfiguration.USART_WordLength=USART_WordLength_8b;

    USARTConfiguration.USART_Parity=USART_Parity_No ;

    USARTConfiguration.USART_HardwareFlowControl=USART_HardwareFlowControl_None;

    USARTConfiguration.USART_Mode=USART_Mode_Rx | USART_Mode_Tx;

    USART_Init(USART2,&USARTConfiguration);

    USART_ITConfig(USART2,USART_IT_RXNE,ENABLE);

    NVIC_EnableIRQ(USART2_IRQn);

    USART_Cmd(USART2,ENABLE);

    GPIOS.GPIO_Mode=GPIO_Mode_AF_PP ;

    GPIOS.GPIO_Speed=GPIO_Speed_50MHz;

    GPIOS.GPIO_Pin=GPIO_Pin_10;

    GPIO_Init(GPIOC,&GPIOS);

    GPIOS.GPIO_Mode=GPIO_Mode_IN_FLOATING ;

    GPIOS.GPIO_Pin=GPIO_Pin_11;

    GPIO_Init(GPIOC,&GPIOS);  

    

    USARTConfiguration.USART_BaudRate=9600;

    USARTConfiguration.USART_StopBits=USART_StopBits_1;

    USARTConfiguration.USART_WordLength=USART_WordLength_8b;

    USARTConfiguration.USART_Parity=USART_Parity_No ;

    USARTConfiguration.USART_HardwareFlowControl=USART_HardwareFlowControl_None;

    USARTConfiguration.USART_Mode=USART_Mode_Rx | USART_Mode_Tx;

    USART_Init(USART3,&USARTConfiguration);

    USART_Cmd(USART3,ENABLE);

Thanks in advance.

#context-context-context
    This topic has been closed for replies.
    parisa
    parisaBest answer
    Associate III
    Mar 1, 2017 3:32 PM UTC
    Posted on March 01, 2017 at 16:32

    Thanks for your comment.

    You are correct and I did some mistake when I wanted to copy my source code , I fix the above problem but still it doesn't work

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2|RCC_APB1Periph_USART3,ENABLE);

    6 replies

    AvaTar
    Senior III
    Mar 1, 2017 3:05 PM UTC
    Posted on March 01, 2017 at 16:05

    RCC_

    APB2

    PeriphClockCmd (RCC_

    APB1

    Periph_USART2|RCC_

    APB1

    Periph_USART3|RCC_APB2Periph_GPIOD |RCC_APB2Periph_GPIOC |RCC_APB2Periph_AFIO,ENABLE);

    Different buses, doesn't match.

    parisa
    parisaAuthorBest answer
    Associate III
    Mar 1, 2017 3:32 PM UTC
    Posted on March 01, 2017 at 16:32

    Thanks for your comment.

    You are correct and I did some mistake when I wanted to copy my source code , I fix the above problem but still it doesn't work

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2|RCC_APB1Periph_USART3,ENABLE);
    Tesla DeLorean
    Guru
    Mar 1, 2017 4:55 PM UTC
    Posted on March 01, 2017 at 16:55

    I don't think you can combine these, split them up

    GPIO_PinRemapConfig(GPIO_Remap_USART2|GPIO_PartialRemap_USART3,ENABLE);

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    parisa
    parisaAuthor
    Associate III
    Mar 1, 2017 4:26 PM UTC
    Posted on March 01, 2017 at 17:26

    Hi,

    Thanks for your contribution

    I split each line with different lines but it doesn't work again

    Tesla DeLorean
    Guru
    Mar 1, 2017 5:32 PM UTC
    Posted on March 01, 2017 at 17:32

    What part specifically are you using? Have you reviewed the Data Sheet and Reference Manuals to make sure the pins and remapping are correct?

    Is this some custom board, or one we should be familiar with? Does anything clash at a pin level that might cause them not to function?

    Post complete testable code as currently compiling.

    #context%20context%20context

    ‌

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    parisa
    parisaAuthor
    Associate III
    Mar 1, 2017 5:12 PM UTC
    Posted on March 01, 2017 at 18:12

    Thanks dear friends for your contribution and sorry for taking your time

    It was my fault that I have reconfigured port c in other part my my program.