Skip to main content
Associate II
Mar 28, 2024 11:58 AM UTC
Question

Two ADC in dual REGULAR SIMULTENIOUS mode

I am trying to run both ADC in dual REGULAR SIMULTENIOUS mode (ADC1 as master and ADC2 as salve) ADC Converted Result shall be stored in an Array Buffer using DMA transfer (single channel only), ADC conversion trigger shall not be software based (we are selecting Tigger Source as TIM1).

i am using STM32G474RE Board.

 

 

This topic has been closed for replies.

2 replies

mƎALLEm
ST Technical Moderator
Mar 28, 2024 12:08 PM UTC

Hello,

What is the question/issue?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Pooja321Author
Associate II
Mar 28, 2024 12:16 PM UTC

Hello ,

I have already been using Triple ADC (ADC1, ADC2, ADC3) in interleaved mode in STM32F407 in another project (It is running perfectly fine), whereas with G4-series same configuration not working as expected.