Skip to main content
Associate II
Oct 16, 2025 3:06 PM UTC
Question

TSOVF not set in VBat mode ?

Hi I'm playing around with the RTC & tamper peripherals of the NUCLEO-H7S3L8. 

I'm wondering if the TSOVF can be set when multiple tampering are detected in VBat mode ? If I'm not mistaken, the RM doesn't say anything against it. However, using the RTC_Tamper example, I notice that it's not the case. When connecting back the main power, the tampering is detected and the timestamp generated corresponds to the first event but TSOVF is not set.

Could anybody confirm that behavior ?

 

Regards.

 

2 replies

Tahm_AAuthor
Associate II
Oct 30, 2025 11:36 AM UTC

Nobody ?

Amel NASRI
ST Technical Moderator
Nov 4, 2025 9:53 AM UTC

Hi @Tahm_A ,

In the product reference manual, the TSOVF description is as following: 

AmelNASRI_0-1762249872201.png

Are you applying this recommendation?

-Amel

 

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.