Skip to main content
JFlowers
Associate III
May 26, 2025
Question

Trying to understand and get Nx_TCP_Echo_Client to work on B-L462E-CELL1

OK, I have a STM32L462RE Discovery Kit (apparently a.k.a. B-L462E-CELL1).

I am trying to get its sole Demonstration application to work (STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client), but I can’t even tell how it is supposed to work.

 

I see “TCP_Echo_Client” in its name, so I assume if I have a simple TCP echo server running on my workstation that if I do the appropriate port forwarding through my router along with the appropriate Windows Firewall settings, then I should see the B-L462E-CELL1 connect to my local TCP Echo Server.

 

Is that correct?


Further, I assume that in this file:

STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\NetXDuo\App\tcp_echo_client.c

I should change TCP_SERVER_PORT from 7 to whatever TCP port my local TCP Echo server is running on, AND I should change the TCP_SERVER_ADDRESS IP_ADDRESS(52,215,34,155) in that same file from 52,215,34,155 (which implies 52.215.34.155) to whatever my public facing router’s WAN address is.

 

Is that correct?


If all of that is right and my SIM card is working right, which I think it is - I’m see messages like this on bootup: “Network is up with IP 10.228.182.49” on TeraTerm - then I should see “10.228.182.49” (or whatever IP address is given my B-L462E-CELL1 on bootup) connect to my local TCP echo server.


Is that correct?


Further, I assume that on my TeraTerm console connected to the B-L462E-CELL1, that I will see some sort of confirmation that my local TCP Echo server replied back to the B-L462E-CELL1 with the exact same message that the B-L462E-CELL1 originally sent to it (to my local TCP echo server).


Is that correct?


Where do I change the message that the B-L462E-CELL1 sends to my local TCP echo server?


Help, please.

 

This topic has been closed for replies.

14 replies

ST Employee
May 27, 2025

Hello @JFlowers ,

 


I see “TCP_Echo_Client” in its name, so I assume if I have a simple TCP echo server running on my workstation that if I do the appropriate port forwarding through my router along with the appropriate Windows Firewall settings, then I should see the B-L462E-CELL1 connect to my local TCP Echo Server.


If your router drops ICMP packets by default, then yes you need to allow them in your firewall settings. To verify this, if you possess two devices connected to the same network, try to ping one device from the other using the command below and see if you get a response or not. If you do, no port-forward or firewall configuration are needed.

ping IP_ADDRESS

 In case you wish to run this application in a Wide Area Network, then you are correct port forward and firewall configuration are needed.

 

Further, I assume that in this file:

STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\NetXDuo\App\tcp_echo_client.c

I should change TCP_SERVER_PORT from 7 to whatever TCP port my local TCP Echo server is running on, AND I should change the TCP_SERVER_ADDRESS IP_ADDRESS (52,215,34,155) in that same file from 52,215,34,155 (which implies 52.215.34.155) to whatever my public facing router’s WAN address is.


Correct.

 

If all of that is right and my SIM card is working right, which I think it is - I’m see messages like this on bootup: “Network is up with IP 10.228.182.49” on TeraTerm - then I should see “10.228.182.49” (or whatever IP address is given my B-L462E-CELL1 on bootup) connect to my local TCP echo server.


Correct.

 

Further, I assume that on my TeraTerm console connected to the B-L462E-CELL1, that I will see some sort of confirmation that my local TCP Echo server replied back to the B-L462E-CELL1 with the exact same message that the B-L462E-CELL1 originally sent to it (to my local TCP echo server).

Is that correct?

Where do I change the message that the B-L462E-CELL1 sends to my local TCP echo server?


I suggest you refer to UM2426 which is dedicated to explaining in detail the the XCube-Cellular package specifically "How to customize the software?" section and let me if it did help you.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
JFlowers
JFlowersAuthor
Associate III
June 2, 2025

I suggest you refer to UM2426 which is dedicated to explaining in detail the the XCube-Cellular package specifically "How to customize the software?" section and let me if it did help you.

 

This document (UM2426) seems to re-enforce my thinking on how this Sample Application is supposed to work.

 

JFlowers
JFlowersAuthor
Associate III
May 28, 2025

This did not work.

 

I successfully ran a TCP Echo server on my local machine and enabled the path through the Internet to it. I turned WiFi off on my cellphone and tested with my cellphone that the TCP Echo server on my local machine was indeed working.

 

I changed the "#define TCP_SERVER_PORT" and "#define TCP_SERVER_ADDRESS IP_ADDRESS" lines in tcp_echo_client.c and re-built Nx_TCP_Echo_Client.bin with STM32CubeIDE.  I dropped Nx_TCP_Echo_Client.bin on the DIS_L462RE drive, allowed it time to install that new FW and then pressed the Reset button on the B-L462E-CELL1 board. 

 

I get traffic like the following in my TeraTerm window, BUT, I get no traffic to my TCP Echo Server on my local machine:

......

......

ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
Cellular interface:
> IP Address: 10.224.94.248
Network is up with IP 10.224.94.248
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync failed.

 

 

 

 

 

 

 

ST Employee
May 28, 2025

Hello,

The SNTP time sync problem is often associated with your application's inability to retrieve NTP server from your ISP's DHCP server, so it switches to manually configurated NTP servers in the application. To solve this, you could try and change the servers' addresses hardcoded in your application in an array called sntp_servers found in app_netxduo.c to ones located in your regions (you could look this information up in your favorite search engine).

 

Some other time, this is due to an optimization issue while compiling the code, you could try and check the optimization level by following these steps:
  • Right click your project name => Properties => C/C++ Build => Settings => In the Tool Settings Tab look for MCU GCC Compiler => Click on Optimization => Select None (-O0) for both Debug and Release Config.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
JFlowers
JFlowersAuthor
Associate III
May 28, 2025

Hi STackPointer64,

All of your comments are very helpful and much appreciated.

I will try your ideas tonight.  I'm not sure they will fix my original problem, but I'm certain they will help on my journey.

 

 

 

 

JFlowers
JFlowersAuthor
Associate III
May 29, 2025

No luck. This did not work either.

 

I set the optimization to None for both Debug and Release new builds and tried the new FW on the board. I still get "SNTP Time Sync failed", if I let it run long enough.

 

I did not change the sntp_servers[] entries. Instead, I checked to see if the existing sntp servers are available at all via:

w32tm /stripchart /computer:X.pool.ntp.org /dataonly
and
sntp commands.

 

0.pool.ntp.org
1.pool.ntp.org
2.pool.ntp.org
3.pool.ntp.org

All responded and showed no errors.

 

However, this "SNTP Time Sync failed" is the least of my worries right now.

This sample code is still not connecting to my TCP Echo Server.

 

JFlowers
JFlowersAuthor
Associate III
May 29, 2025

Should this exact same sample application (STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client) and exact same FW binary (Nx_TCP_Echo_Client.bin) work on a P-L496G-CELL02 too, without me having to recompile/rebuild it?

 

JFlowers
JFlowersAuthor
Associate III
May 31, 2025

> In case you wish to run this application in a Wide Area Network, then you are correct port forward and firewall

> configuration are needed.

 

I don't see or understand how we can run this application in a Local Area Network.  The cellular connection is always going to be coming from the outside (WAN), right?

 

---

 

ST Employee
June 2, 2025

Hello, 

I don't see or understand how we can run this application in a Local Area Network.  The cellular connection is always going to be coming from the outside (WAN), right?


Apologies for the oversight! You’re right, I was focused on the fact that the project is a TCP echo client and overlooked the cellular aspect.

Since the SNTP issue is resolved, the most probable problem could be that your firewall/router is blocking the incoming connection from the TCP echo client. Could you verify that the port used is properly forwarded in your router and the Inbound rules allow for communication through that port. Check also if there is possibly any other service utilizing that port in your network.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
JFlowers
JFlowersAuthor
Associate III
June 4, 2025


(Well, I sent this more than 13.5 hours ago. Let’s see if it goes through this time.)


Hi @STackPointer64,


1.
When I connect to my local TCP Echo Server using my cellphone (with WiFi turned off), this is what I get:

C:\joe\TCPechoServerWs\Release>TCPEchoServerWS.exe 50001

Handling client (174.203.246.247):
hello STackPointer64!
C:\joe\TCPechoServerWs\Release>

---

2.
When I turn on the B-L462E-CELL1 by plugging it into a USB port, I get nothing. It just sits there:

C:\joe\TCPechoServerWs\Release>TCPEchoServerWS.exe 50001

---

3.
In my tcp_echo_client.c file,

\en.stm32cubeexpansion-cellular-v7-1-0\STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\NetXDuo\App\tcp_echo_client.c

\en.stm32cubeexpansion-cellular-v7-1-0\STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\STM32CubeIDE\Debug\Nx_TCP_Echo_Client.bin

This is what I have changed and recompiled and dropped Nx_TCP_Echo_Client.bin on the “DISL462RE (E:)” drive for flashing:


#ifndef TCP_SERVER_PORT
#define TCP_SERVER_PORT 50001
#endif /* TCP_SERVER_PORT */

#ifndef TCP_SERVER_ADDRESS
#define TCP_SERVER_ADDRESS IP_ADDRESS(<MY_ROUTER’s>,<WAN>,<IP>,<ADDRESS>)
#endif /* TCP_SERVER_ADDRESS */


---

4.
This is what I get when I power on the B-L462E-CELL1:


ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #1: channel=1 / errorId=7 / gravity=2
LOG ERROR #2: channel=2 / errorId=1 / gravity=2
STM32 IP Address: 0.0.0.0
DNS Server address: 8.8.8.8
SNTP Time Sync... 0.pool.ntp.org
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #3: channel=1 / errorId=7 / gravity=2
LOG ERROR #4: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
LOG ERROR #5: channel=1 / errorId=7 / gravity=2
LOG ERROR #6: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
ATCModem:no pending URC
ATCModem:Tempo started (2000 ms)...
ATCore:TIMEOUT EVENT(2000 ms)
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModck:<MAX SIZE INFO> msgtype=4 size=0 (biggest =78)ATCModem:NetworkState (EPS) = UNKNOWN
ATCModem:+CEREG: tac=3007 =0xbbf
ATCModem:+CEREG: ci=7 =0x7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG URC: lac=9997 =0x270d
ATCModem:+CREG URC: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
Cellular interface:
> IP Address: 10.229.79.126
Network is up with IP 10.229.79.126
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
...
...

---

5.
This is what I get when I press the RESET button on the B-L462E-CELL1 board:

Nx_TCP_Echo_Client application started.
Create IP instance...

===== X-Cube-Cellular version : X-CUBE-CELLULAR-7.1.0 =====

TYPE1SC UART config: BaudRate=115200 / HW flow ctrl=1
Get IP Address...
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #1: channel=1 / errorId=7 / gravity=2
LOG ERROR #2: channel=2 / errorId=1 / gravity=2
STM32 IP Address: 0.0.0.0
DNS Server address: 8.8.8.8
SNTP Time Sync... 0.pool.ntp.org
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #3: channel=1 / errorId=7 / gravity=2
LOG ERROR #4: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
LOG ERROR #5: channel=1 / errorId=7 / gravity=2
LOG ERROR #6: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
ATCModem:no pending URC
ATCModem:Tempo started (2000 ms)...
ATCore:TIMEOUT EVENT(2000 ms)
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModck:<MAX SIZE INFO> msgtype=4 size=0 (biggest =78)ATCModem:NetworkState (EPS) = UNKNOWN
ATCModem:+CEREG: tac=3007 =0xbbf
ATCModem:+CEREG: ci=7 =0x7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG URC: lac=9997 =0x270d
ATCModem:+CREG URC: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
Cellular interface:
> IP Address: 10.230.16.255
Network is up with IP 10.230.16.255
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
...
...


---

6.
Still, my local TCP Echo Server gets no connections.

---

7.
Help, please.

 

JFlowers
JFlowersAuthor
Associate III
June 4, 2025

(Well, I sent this more than 13.5 hours ago. Let’s see if it goes through this time.)


Hi @STackPointer64,


1.
When I connect to my local TCP Echo Server using my cellphone (with WiFi turned off), this is what I get:

C:\joe\TCPechoServerWs\Release>TCPEchoServerWS.exe 50001

Handling client (174.203.246.247):
hello STackPointer64!
C:\joe\TCPechoServerWs\Release>

---

2.
When I turn on the B-L462E-CELL1 by plugging it into a USB port, I get nothing. It just sits there:

C:\joe\TCPechoServerWs\Release>TCPEchoServerWS.exe 50001

---

3.
In my tcp_echo_client.c file,

\en.stm32cubeexpansion-cellular-v7-1-0\STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\NetXDuo\App\tcp_echo_client.c

\en.stm32cubeexpansion-cellular-v7-1-0\STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\STM32CubeIDE\Debug\Nx_TCP_Echo_Client.bin

This is what I have changed and recompiled and dropped Nx_TCP_Echo_Client.bin on the “DISL462RE (E:)” drive for flashing:


#ifndef TCP_SERVER_PORT
#define TCP_SERVER_PORT 50001
#endif /* TCP_SERVER_PORT */

#ifndef TCP_SERVER_ADDRESS
#define TCP_SERVER_ADDRESS IP_ADDRESS(<MY_ROUTER’s>,<WAN>,<IP>,<ADDRESS>)
#endif /* TCP_SERVER_ADDRESS */


---

4.
This is what I get when I power on the B-L462E-CELL1:


ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #1: channel=1 / errorId=7 / gravity=2
LOG ERROR #2: channel=2 / errorId=1 / gravity=2
STM32 IP Address: 0.0.0.0
DNS Server address: 8.8.8.8
SNTP Time Sync... 0.pool.ntp.org
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #3: channel=1 / errorId=7 / gravity=2
LOG ERROR #4: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
LOG ERROR #5: channel=1 / errorId=7 / gravity=2
LOG ERROR #6: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
ATCModem:no pending URC
ATCModem:Tempo started (2000 ms)...
ATCore:TIMEOUT EVENT(2000 ms)
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModck:<MAX SIZE INFO> msgtype=4 size=0 (biggest =78)ATCModem:NetworkState (EPS) = UNKNOWN
ATCModem:+CEREG: tac=3007 =0xbbf
ATCModem:+CEREG: ci=7 =0x7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG URC: lac=9997 =0x270d
ATCModem:+CREG URC: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
Cellular interface:
> IP Address: 10.229.79.126
Network is up with IP 10.229.79.126
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
SNTP Time Sync... 3.pool.ntp.org
SNTP Time Sync... 0.pool.ntp.org
...
...

---

5.
This is what I get when I press the RESET button on the B-L462E-CELL1 board:

Nx_TCP_Echo_Client application started.
Create IP instance...

===== X-Cube-Cellular version : X-CUBE-CELLULAR-7.1.0 =====

TYPE1SC UART config: BaudRate=115200 / HW flow ctrl=1
Get IP Address...
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #1: channel=1 / errorId=7 / gravity=2
LOG ERROR #2: channel=2 / errorId=1 / gravity=2
STM32 IP Address: 0.0.0.0
DNS Server address: 8.8.8.8
SNTP Time Sync... 0.pool.ntp.org
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 0
LOG ERROR #3: channel=1 / errorId=7 / gravity=2
LOG ERROR #4: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
LOG ERROR #5: channel=1 / errorId=7 / gravity=2
LOG ERROR #6: channel=2 / errorId=1 / gravity=2
SysCtrl_TYPE1SC:modem channel closed
SysCtrl_TYPE1SC:MODEM POWER OFF
SysCtrl_TYPE1SC:MODEM POWER ON
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCore:TIMEOUT EVENT(1000 ms)
SysCtrl_TYPE1SC:UART config: setting HW Flow Control to 1
ATCModem:Tempo started (3000 ms)...
ATCore:TIMEOUT EVENT(3000 ms)
Modem Boot OK, sim slot nb 1
ATCModem:no pending URC
ATCModem:Tempo started (2000 ms)...
ATCore:TIMEOUT EVENT(2000 ms)
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (CS) = NOT_REGISTERED_NOT_SEARCHING
ATCModem:NetworkState (EPS) = NOT_REGISTERED_SEARCHING
ATCModck:<MAX SIZE INFO> msgtype=4 size=0 (biggest =78)ATCModem:NetworkState (EPS) = UNKNOWN
ATCModem:+CEREG: tac=3007 =0xbbf
ATCModem:+CEREG: ci=7 =0x7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG URC: lac=9997 =0x270d
ATCModem:+CREG URC: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
ATCModem:NetworkState (EPS) = REGISTERED_HOME_NETWORK
ATCModem:+CEREG: tac=9997 =0x270d
ATCModem:+CEREG: ci=197108497 =0xbbfa311
ATCModem:+CEREG: act=7
ATCModem:NetworkState (CS) = REGISTERED_HOME_NETWORK
ATCModem:+CREG: lac=9997 =0x270d
ATCModem:+CREG: ci=197108497 =0xbbfa311
Cellular interface:
> IP Address: 10.230.16.255
Network is up with IP 10.230.16.255
SNTP Time Sync... 1.pool.ntp.org
SNTP Time Sync... 2.pool.ntp.org
...
...


---

6.
Still, my local TCP Echo Server gets no connections.

---

7.
Help, please.

ST Employee
June 5, 2025

Hello,

After analyzing the output log you provided for the different test cases and comparing it with the application source code and program flow, it appears that the issue revolves around SNTP time synchronization. This step is critical, as it is the last initialization step required before starting the TCP Echo Client thread, as shown in the program flow below.

 /* Sync up time by SNTP at start up. */
 ret = sntp_time_sync();

 /* Check status. */
 if (ret != NX_SUCCESS)
 {
 printf("SNTP Time Sync failed.\r\n");
 Error_Handler();
 }

 /* Start sample. */
 sample_start(&IpInstance, &AppPool, &DnsClient, unix_time_get);

 /* this thread is not needed any more, we relinquish it */
 tx_thread_relinquish();
}

To further investigate and resolve the issue, follow these steps:

  1. Use Wireshark for Packet Analysis:
    Install and run Wireshark on your PC to monitor the network interface being used. Filter the traffic to focus on packets coming from the board's IP address. Check if:

    • Packets are being received and dropped or not reaching your PC.
  2. Test with a Clean Project:
    To eliminate any potential issues caused by source code modifications:

    • Obtain a fresh, unmodified project.
    • Change only the server IP and server port to match your setup.
    • Compile the project without making any other changes.
      This will help ensure the issue is not caused by unintended changes in the code.
  3. Change the NTP Server List:
    If the above steps do not resolve the issue, try modifying the NTP server list in the source code. Use reliable and accessible NTP servers to ensure proper synchronization. You could use NTP Pool project .

  4. Adjust NX_SNTP_CLIENT_MAX_ROOT_DISPERSION:
    If none of the above steps work, locate the NX_SNTP_CLIENT_MAX_ROOT_DISPERSION parameter in the nx_user.h file. This parameter measures the precision of the server clock. Set it to 0 to disable this feature and test the setup again.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.
JFlowers
JFlowersAuthor
Associate III
June 9, 2025


Hi @STackPointer64,


I had to REM-out the call to sntp_time_sync() in app_netxduo.c and then use the PavelBansky EchoTool. It “worked” after that.

My bet is that the SNTP service is not allowed/not enabled in the cellular connection provider’s network (TRUPHONE).

---

\en.stm32cubeexpansion-cellular-v7-1-0\STM32CubeExpansion_CELLULAR_V7.1.0\Projects\B-L462E-CELL1\Demonstrations\Nx_TCP_Echo_Client\NetXDuo\App\app_netxduo.c

// /* Sync up time by SNTP at start up. */
// ret = sntp_time_sync();
//
// /* Check status. */
// if (ret != NX_SUCCESS)
// {
// printf("SNTP Time Sync failed.\r\n");
// Error_Handler();
// }

---

https://github.com/PavelBansky/EchoTool
C:\joe\TCPechoServerWs\Release>"C:\Users\joefl\Downloads\echotool.exe" /p tcp /s 50001

SHA256 hash of C:\Users\joefl\Downloads\echotool.exe:
e1af7723d0672d7169cd259829b743efb0b9ae297276687a063e6853aee55733

---


1. Use Wireshark for Packet Analysis
Unnecessary


2. Test with a Clean Project
Unnecessary


3. Change the NTP Server List
I tried the following, but it did not help.

static const char *sntp_servers[] =
{
“0.europe.pool.ntp.org”,
“1.europe.pool.ntp.org”,
“2.europe.pool.ntp.org”,
“3.europe.pool.ntp.org”
};

and

static const char *sntp_servers[] =
{
"0.north-america.pool.ntp.org",
"1.north-america.pool.ntp.org",
"2.north-america.pool.ntp.org",
"3.north-america.pool.ntp.org"
};

I tried those two in particular because the IP addresses that were connecting to my local TCP echo server (with sntp_time_sync() REM-ed out) seemed to be located in the UK or in the US.

Still, sntp_time_sync() did not work.


4. Adjust NX_SNTP_CLIENT_MAX_ROOT_DISPERSION

I tried Adjust NX_SNTP_CLIENT_MAX_ROOT_DISPERSION = 0 as you recommended, but it did not help.

---