Skip to main content
Visitor II
July 21, 2024
Question

Trying to print "Hello World" NUCLEO-L4R5ZI with ST-Link SWD

Hi everyone,

 

I am new to the embedded world and I currently have a STM32 Nucleo L4R5ZI board. I am trying to print "Hello World" to the SWV ITM Data Console through port 0. I am following the Fastbit tutorial on Udemy which uses a STM32F407VG board.

 

I created a empty project that doesn't use any HALs or generated code from the CubeMX software. I included the stdio.h header file and have the printf("Hello World\n"); in the main loop of main.c file:

 

#include <stdint.h>
#include <stdio.h>


#if !defined(__SOFT_FP__) && defined(__ARM_FP)
 #warning "FPU is not initialized, but the project is compiling for an FPU. Please initialize the FPU before use."
#endif

int main(void)
{

	printf("Hello World\n");
 /* Loop forever */
	for(;;);
}

 

 

In the syscalls.c files, I created a new function as stated below which I got from the tutorial:

 

 

//Debug Exception and Monitor Control Register base address
#define DEMCR 			*((volatile uint32_t*) 0xE000EDFCU )

/* ITM register addresses */
#define ITM_STIMULUS_PORT0 	*((volatile uint32_t*) 0xE0000000 )
#define ITM_TRACE_EN 	*((volatile uint32_t*) 0xE0000E00 )

void ITM_SendChar(uint8_t ch)
{

	//Enable TRCENA
	DEMCR |= ( 1 << 24);

	//enable stimulus port 0
	ITM_TRACE_EN |= ( 1 << 0);

	// read FIFO status in bit [0]:
	while(!(ITM_STIMULUS_PORT0 & 1));

	//Write to ITM stimulus port0
	ITM_STIMULUS_PORT0 = ch;
}

 

 

 

I then changed my write function as well:

 

 

__attribute__((weak)) int _write(int file, char *ptr, int len)
{
 (void)file;
 int DataIdx;

 for (DataIdx = 0; DataIdx < len; DataIdx++)
 {
// __io_putchar(*ptr++);
	 ITM_SendChar(*ptr++);
 }
 return len;
}

 

 

 

I then created a debug configuration using the following settings:
Screenshot 2024-07-20 212012.png

I then open the debugger and have a SWV ITM Data Console with port 0 enabled and have the trace started. When I run the code, nothing appears on the console. 

 

What could be the issue? I thought it was an issue with the registers, but I verified the ITM_STIMULUS_PORT0 
 and ITM_TRACE_EN registers. I couldn't find the address for the DEMCR register.

 

Any help with be greatly appreciated!

 

 

This topic has been closed for replies.

4 replies

Associate II
November 15, 2024

Hi,

The ST-link section of my board completely shuts down including the RGB LED on my Nucleo-F207ZG when I try similar. Does your debugger appear to be alive at all?

Tesla DeLorean
Guru
November 15, 2024

Make sure the Core Clock reflects the speed you're running the part

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate II
November 16, 2024

Hi,

 

Thanks. I checked the clock configuration page and used live expressions to view the speed.

I got 160mhz, then 96mhz(after it config'd I guess) from the live expressions.

Where exactly in the clock config page should I get my value from?

Thanks.

Tesla DeLorean
Guru
November 16, 2024

Isn't max 120 MHz? HSI running out of start, probably 16 MHz

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..