Skip to main content
arthurg
Associate II
June 30, 2011
Question

Trying to boot from bootloader in STML152 although not present

  • June 30, 2011
  • 4 replies
  • 913 views
Posted on June 30, 2011 at 23:11

I am doing a STM32L152 design, using IAR tools, and have run into problems with JTAG programming. My code resides in Flash, and sometimes there is a JTAG ''no communication'' problem which prevents me from programming. Everything locks up. I was advised to try another boot mode to force it to communicate. I have used system bootload, except there is no bootloader according to the errata sheet.

Does anyone know what happens when there is this attempt?

Secondarily, does anyone know what clock selection is invoked in this mode - what speed?

    This topic has been closed for replies.

    4 replies

    infoinfo989
    Associate III
    July 1, 2011
    Posted on July 01, 2011 at 07:16

    What JTAG device are you using? IAR doesn't support all the JTAG dongles equally well. Have you tried using a different dedicated programming utility for your JTAG dongle?

    arthurg
    arthurgAuthor
    Associate II
    July 1, 2011
    Posted on July 01, 2011 at 07:52

    I am using the J-Link Ultra. It was tech support at IAR who suggested forcing a boot from another space than Flash.

    js23
    Associate III
    July 1, 2011
    Posted on July 01, 2011 at 10:35

    There have always been problems for me to connect to a device after a reset when one of the sleep modes is used. I assume, that you are using sleep modes, too (would not make much sense to use a STM32L without....)

    My workaround: When debugging, I always insert a delay after reset or wait for a switch before going to sleep for the first time.

    Besides that, everything works quite well. I use IAR or Atollic with ST-Link and SWD. The only thing I discovered until now: The debugger connection gets lost when running the CPU on MSI with clock frequencies below 256kHz.

    Tesla DeLorean
    Guru
    July 1, 2011
    Posted on July 01, 2011 at 13:39

    There have always been problems for me to connect to a device after a reset...

    I think it's even more general than that, it's more to do with the thousands of cycles the JTAG is taking to wrestle control after the reset. As you said putting in a loop or doing some busy work first will mitigate it somewhat, and most JTAG pods have several options/configurations for the boot/reset strategies to use.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..