Skip to main content
PANAN.1
Associate
October 21, 2021
Question

try to communicate between Two STM32 F407 discovery board in I2C Protocol but slave not work properly it gives no output

master side :

uint8_t TMP102_ADDR = 0x08;

uint8_t REG_TEMP = 0x01;

int result = 0x01;

(result is numerical data which i want to transfer to another stm 32 )

 HAL_I2C_Master_Transmit(&hi2c3,(TMP102_ADDR<<1),&result,sizeof(result),100);

slave side stm 32 program

uint8_t TMP102_ADDR = 0x08; // Use 8-bit address

uint8_t REG_TEMP = 0x00;

char buf[4];

AL_I2C_Mem_Read(&hi2c1,(TMP102_ADDR<<1),0x0C,I2C_MEMADD_SIZE_8BIT,buf, I2C_MEMADD_SIZE_8BIT,100);

still it shows error or no output on slave side both supplied by USB and ground at common point

This topic has been closed for replies.

5 replies

TDK
October 21, 2021

The slave should call HAL_I2C_Slave_Receive to receive the information from the master.

There are examples for this. Here is one:

https://github.com/STMicroelectronics/STM32CubeF4/blob/2f3b26f16559f7af495727a98253067a31182cfc/Projects/STM32F412ZG-Nucleo/Examples/I2C/I2C_TwoBoards_ComPolling/readme.txt

"If you feel a post has answered your question, please click ""Accept as Solution""."
PANAN.1
PANAN.1Author
Associate
October 22, 2021

HAL_I2C_Slave_Receive(&hi2c1,(uint8_t *)aRxBuffer,sizeof(aRxBuffer), 1000);

i use this instruction also but not works....

TDK
October 22, 2021

It won't even compile as you don't have a slave address. Were you able to follow the example?

"If you feel a post has answered your question, please click ""Accept as Solution""."
PANAN.1
PANAN.1Author
Associate
October 23, 2021

i see the example but still it not work for my case

i have same stm32 f407 discovery board as tx and rx side and adress is 0x08

PANAN.1
PANAN.1Author
Associate
October 23, 2021

yes thank you now its work

but it dnt send updated value of ADC from transmit side

receiving side get value only once

it not update time by time