Skip to main content
stm322399
Senior
May 20, 2016
Question

Troubles using Mx plugin

Posted on May 20, 2016 at 10:19

Hi folks,

I have installed MX plugin 4.14.0.201603171736 into an existing eclipse Mars.2 (4.5.2). Looks like it worked.

But when I try to show an STM32CubeMX window, it simply crashes my eclipse.

I was expecting being able to edit a customer supplied .ioc file.

Is this possible ?

Is this plugin known to work with Mars.2 ?

Thanks for clarifications.
    This topic has been closed for replies.

    1 reply

    stm322399
    stm322399Author
    Senior
    May 20, 2016
    Posted on May 20, 2016 at 14:06

    For those interrested in, a short log is pasted hereafter.

    On my side I downloaded the standalone application which just work fine.

    #
    # A fatal error has been detected by the Java Runtime Environment:
    #
    # SIGSEGV (0xb) at pc=0xed9d335f, pid=7025, tid=4149466880
    #
    # JRE version: OpenJDK Runtime Environment (7.0_91-b02) (build 1.7.0_91-b02)
    # Java VM: OpenJDK Client VM (91-b01 mixed mode, sharing linux-x86 )
    # Derivative: IcedTea 2.6.3
    # Distribution: Debian GNU/Linux 8.2 (jessie), package 7u91-2.6.3-1~deb8u1
    # Problematic frame:
    # C [libgdk-x11-2.0.so.0+0x4735f] gdk_display_open+0x4f
    #
    # Failed to write core dump. Core dumps have been disabled. To enable core dumping, try ''ulimit -c unlimited'' before 
    #
    # If you would like to submit a bug report, please include
    # instructions on how to reproduce the bug and visit:
    # http://icedtea.classpath.org/bugzilla
    # The crash happened outside the Java Virtual Machine in native code.
    # See problematic frame for where to report the bug.
    #