Troubles setting up the CAN
Hi,
I'm having troubles setting up the CAN bus on my STM32F103R4. I'm using the can example from the keil homepage . When it is about to leave initialization mode, hardware doesnt reset the INAK bit in MSR register and I really don't know why. Here's the relevant slice of the code:void
CAN_setup (void
) {unsigned
int
brp = stm32_GetPCLK1(); RCC->APB1ENR |= RCC_APB1ENR_CANEN;// enable clock for CAN
// Note: MCBSTM32 uses PB8 and PB9 for CAN
RCC->APB2ENR |= RCC_APB2ENR_AFIOEN;// enable clock for Alternate Function
AFIO->MAPR &=0xFFFF9FFF
;// reset CAN remap
AFIO->MAPR |=0x00004000
;// set CAN remap, use PB8, PB9
RCC->APB2ENR |= RCC_APB2ENR_IOPBEN;// enable clock for GPIO B
GPIOB->CRH &= ~(0x0F
<<0
); GPIOB->CRH |= (0x08
<<0
);// CAN RX pin PB.8 input push pull
GPIOB->CRH &= ~(0x0F
<<4
); GPIOB->CRH |= (0x0B
<<4
);// CAN TX pin PB.9 alternate output push pull
NVIC->ISER[0
] |= (1
<< (USB_HP_CAN_TX_IRQChannel &0x1F
));// enable interrupt
NVIC->ISER[0
] |= (1
<< (USB_LP_CAN_RX0_IRQChannel &0x1F
));// enable interrupt
CAN->MCR = (CAN_MCR_NART | CAN_MCR_INRQ);// init mode, disable auto. retransmission
// Note: only FIFO 0, transmit mailbox 0 used
CAN->IER = (CAN_IER_FMPIE0 | CAN_IER_TMEIE);// FIFO 0 msg pending, Transmit mbx empty
/* Note: this calculations fit for PCLK1 = 36MHz */
brp = (brp /18
) /500000
;// baudrate is set to 500k bit/s
/* set BTR register so that sample point is at about 72% bit time from bit start */
/* TSEG1 = 12, TSEG2 = 5, SJW = 4 => 1 CAN bit = 18 TQ, sample at 72% */
CAN->BTR &= ~(((0x03
) <<24
) | ((0x07
) <<20
) | ((0x0F
) <<16
) | (0x1FF
)); CAN->BTR |= ((((4
-1
) &0x03
) <<24
) | (((5
-1
) &0x07
) <<20
) | (((12
-1
) &0x0F
) <<16
) | ((brp-1
) &0x1FF
)); }void
CAN_testmode (unsigned
int
testmode) { CAN->BTR &= ~(CAN_BTR_SILM | CAN_BTR_LBKM);// set testmode
CAN->BTR |= (testmode & (CAN_BTR_SILM | CAN_BTR_LBKM)); }void
CAN_start (void
) { CAN->MCR &= ~CAN_MCR_INRQ;// normal operating mode, reset INRQ
while
(CAN->MSR & CAN_MCR_INRQ); } I hope somebody knows how to fix that! Regards. Alex