Skip to main content
infoinfo983
Associate III
May 10, 2018
Question

Transmission problem with UART7 and DMA on the STM32H743-Nucleo144 demoboard.

  • May 10, 2018
  • 0 replies
  • 520 views
Posted on May 10, 2018 at 14:16

Hello everyone,

I am trying to transmit a string with the UART7 with the DMA on a STM32H743-NUCLEO144 demoboard, to do this I have shorted the pins PF6 and PF7 on the Morpho connector CN11 (short circuit between TX and RX of the UART7). I initialized the components and tried to send a string to DMA, but nothing is transmitted.

What did I do wrong?

I enclose complete project for Atollic 9.0.0.

Thank you
    This topic has been closed for replies.