Skip to main content
danesh
Associate III
April 28, 2016
Question

Transferring large blocks of data over USART

  • April 28, 2016
  • 2 replies
  • 644 views
Posted on April 28, 2016 at 15:20

Dear all,

I have problem transferring relatively large block data (>= 600 bytes) over USART. All blocks smaller than 600 bytes can be sent successfully from MCU and the host at the other end receives that correctly. I have the following routine with some timeout to send the data from MCU to the host:

static void send_response(uint8_t *response,

                          uint16_t frame_length) {

  for (int i = 0; i < frame_length; ++i) {

    USART_SendData(UART4, response[i]);

    timer.Start(TIMEOUT);

    while ((!timer.iselapsed()) &&

           (USART_GetFlagStatus(UART4, USART_FLAG_TC) == RESET));

  }

}

The logic seems to be pretty simple but it doesn't work for large frames and it seems that the USART_FLAG_TC is never set so the communication will not be successful. The limit of 600 bytes seems to be very low so I am almost sure that I am doing something wrong. Any help is highly appreciated.

Regards,

Dan
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    April 28, 2016
    Posted on April 28, 2016 at 15:29

    I'd front check TXE, back checking TC is the slowest possible method.

    Does it work without your time out method if you check TXE before sending each byte? It it only fails with your time out, then review the math there.

    The USART may also break if you park a debug view over the peripheral.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    danesh
    daneshAuthor
    Associate III
    April 28, 2016
    Posted on April 28, 2016 at 17:40

    Thank you very much clive1. I changed the check to front TXE and got some speedup. The problem is solved now and it happened because I had forgotten to kick the watchdog in the sending loop. This bug didn't show up before because the data that I used to send/received was small, but when the data is large, the watchdog needs to be kicked.

    Thanks again,

    Dan