Skip to main content
Associate II
December 10, 2025
Solved

toolchain installation failures

Hi.  I have a newly purchased NUCLEO-U575ZI-Q.  I followed the instructions here to install the toolchain on Windows 11:

https://www.st.com/en/evaluation-tools/nucleo-u575zi-q.html#documentation

https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step1_Tools_installation

After one unsuccessful attempt where I chose my own installation folders, I uninstalled everything and took the defaults.

What a mess!  The default installation folders are spread between AppData, Program Files, and C:\ST.  But OK, if that's what it takes.

Unfortunately, I got to step 5 and found that the instructions diverge from reality.

mdeis_0-1765389725567.png

They never said to click Finish to complete the Import Projects dialog.  And there is no way to select the project they mention from it.  But if I click Finish, then a tiny icon appears on the upper left.  If I click it, then there is a Project Explorer window.

The next step is:

mdeis_1-1765390093122.png

My IDE has no Debug icon (the the little yellow blob on its lower left).  But it does have a Debug As icon.  Clicking that one results in:

mdeis_2-1765390153742.png

So now I'm stuck.

Any help would be greatly appreciated!

Thanks,

Mike

 

AScha.3
AScha.3Best answer
Super User
December 12, 2025

Hi,

which version IDE you installed ?

+

Did you try, what i wrote ? (1. load/install IDE 1.19.  (yes..ok...etc. , as it wants.) ....)

If you feel a post has answered your question, please click on " Best Answer ".

8 replies

KnarfB
Super User
December 10, 2025

"The selection cannot be launched..." refers to the selection in the Project Explorer View. Make sure that the project icon of the project you want to debug is selected. 

UM2609 STM32CubeIDE user guide may also be helpful.

hth

KnarfB

mdeisAuthor
Associate II
December 11, 2025

mdeis_0-1765466825176.png

The project was indeed selected.

So it seems that was not the issue.

Mike

 

AScha.3
Super User
December 10, 2025

Hi,

this is not an Arduino: click on anything and it works somehow. :)

1. load/install IDE 1.19.  (yes..ok...etc. , as it wants.)

2. start new stm32 project...select your chip U575 or board nuc..-575... give name etc...see chip pin layout.

3. then do/create what you want, set clock tree to something useful, click generate code...and compile/debug...

You will have to learn a lot, but in the end you can create, what you imagine ..within the limits of selected chip.

If you feel a post has answered your question, please click on " Best Answer ".
mdeisAuthor
Associate II
December 11, 2025

Hello AScha.3,

I'm not trying to create a new project from scratch.

I'm trying to run one of the predefined examples (I'm following the official tools installation steps here:  https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step1_Tools_installation).

Even though it's not an Arduino, is it too much to expect that one of the provided examples for the NUCLEO-U575ZI-Q should come ready to compile?

It's a serious question.

As the installation steps suggest, I got the example from STM32CubeMX:

mdeis_1-1765467516508.png

mdeis_2-1765467543049.png

All the examples then showed up here:

 

mdeis_4-1765467664587.png

The tools installation steps suggest that one should be able to simply click "Debug" and run the example on the device (assuming driver installation succeeded).

Should I not expect the installation documentation to be true?

Thanks.

Mike

 

AScha.3
AScha.3Best answer
Super User
December 12, 2025

Hi,

which version IDE you installed ?

+

Did you try, what i wrote ? (1. load/install IDE 1.19.  (yes..ok...etc. , as it wants.) ....)

If you feel a post has answered your question, please click on " Best Answer ".
mdeisAuthor
Associate II
December 11, 2025

BTW, the instructions say:

mdeis_0-1765469457741.png

But on my board, the CN2 header is not populated:

mdeis_1-1765469549073.png

And there are four leads!  What should be jumpered to what?

The board documentation (um2861) makes no mention of it.

Thanks.

Mike

 

AScha.3
Super User
December 11, 2025

>But on my board, the CN2 header is not populated:

right, see circuit of board:

https://www.st.com/resource/en/schematic_pack/mb1549-u575ziq-c05-schematic.pdf

 

AScha3_0-1765471923159.png

its for programming the st-linl itself - you should never need it.

If you feel a post has answered your question, please click on " Best Answer ".
mdeisAuthor
Associate II
February 19, 2026

Looks like it was purely a 2.0 issue.

Version 1.19 works as expected.

Thanks.

 

--Mike

P.S. sorry it took so long to reply.  I had moved on to other tasks, and since I'm not getting notifications from the message board, missed your reply.