To wich parameter refers HSE oscillator characteristic Gm in STM32L443 datasheet on page 123? Does it refer to AN2867 parameter gm or to Gm_crit_max?
I'm in doubt about the transconductance parameter of the HSE oscillator in STM32L443.
To select an appropriate cristal I studied AN2867.
If the datasheet of STM32L443 which notes "Gm = 1.5mA/V" refers to gm the transconductance of the passive elements should stay below 0.3mA/V, which is really low. Selecting a crystal with appropriate characteristics will result in one with a low load capacitance, so I have trouble to even place load capacitors beside the cristal. If I take the PCB and I/O-stray capacitance to have 10pF the load capacitors should then have negative values (obviously this is impossible).
But if "Gm = 1.5mA/V" refers to Gm_crit_max then the transconductance of the passive components must only be less than this (not 5 times smaller).
Can please someone give advice here?
May there should be a naming convention about characteristics?!
Thanks a lot
Christoph