Skip to main content
Senior
August 20, 2024
Question

Timer triggered SPI transfer with data size beyond 64k bytes

Hi,

With GPDMA standard mode, I implemented timer triggered SPI DMA transfer. But the 'Size' argument of the 'HAL_SPI_TransmitReceive_DMA()' is 'unit16_t', this means it can only transfer 64k bytes once. Are there any method to transfer beyond this value using DMA?

Thanks.

This topic has been closed for replies.

4 replies

Bob S
Super User
August 20, 2024

If your total transfer size is always a multiple of 2, you can change the SPI config to 16-bit data instead of 8-bit.  Then you get 64K 16-bit words, or 128K bytes per call.

Or just use the transfer complete callback to start a 2nd (or 3rd) transfer of the next chunk of data.

divergerAuthor
Senior
August 21, 2024

Hi,

It seems there are something not clear now.

  1. For the SPI transfer APIs without '_DMA' suffix, they all accept an 16-bit 'Size', which mean the 'number of' transfers. That means they are counted in 'transfers', but not bytes. I think I can enlarge the size of one single transfer to 'halfword', 'word', to increase the total bytes it can transfer.
  2. For the APIs with '_DMA' suffix, the 'Size' is multiplied by the 'SPI_DATASIZE' in bytes, then passed to the DMA's CBR1 register (the BNDT[15:0]) field. This is the final cause of the 64k bytes limitation.

So, I think the question now is how to break the 64k bytes limitation of GPDMA. Right?

 

Thanks.

MasterT
Lead II
August 21, 2024

I remember a decade ago I write my own code for Atmel's SAM3X uCPU, that supports DMA Link List mode.  No driver from IC makers at that time. I see similar situation here, DMA has feature LList but spi_dma_transfer has no reference in HAL.  Probaly, it's quite possible to create two lists and link them in circle, at least I see dma_hal has some references to LList type definition structure