Skip to main content
nanayakkaraan
Associate III
October 20, 2010
Question

Timer interrupt

  • October 20, 2010
  • 4 replies
  • 1082 views
Posted on October 20, 2010 at 11:55

Timer interrupt

    This topic has been closed for replies.

    4 replies

    vmtetons
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 14:11

    Hi ANN

    Could you please let me know where you got your STM32L152 devices or board from.  I do not seem to find any distributor here in the US for teh low power family.

    Thanks

    stmdesi

    andy239955_stm1_stmicro_com
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 14:11

    Hi ANN,

    I have some bits using TIM1 on a ST..103.. that may help. These use the standard libraries.

    Put this somewhere in your main.

       NVIC_InitTypeDef             NVIC_InitStructure;

       TIM1_TimeBaseInitTypeDef     TIM1_TimeBaseInitStruct;

       RCC_APB2PeriphClockCmd (RCC_APB2Periph_TIM1, ENABLE);

          // Set timer1

       TIM1_TimeBaseInitStruct.TIM1_Prescaler = 8; 

       TIM1_TimeBaseInitStruct.TIM1_CounterMode = TIM1_CounterMode_Up;

       TIM1_TimeBaseInitStruct.TIM1_Period = 10000;

       TIM1_TimeBaseInitStruct.TIM1_ClockDivision = TIM1_CKD_DIV1;

       TIM1_TimeBaseInitStruct.TIM1_RepetitionCounter = 0;

       TIM1_TimeBaseInit (&TIM1_TimeBaseInitStruct);

       NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQChannel;

       NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 9;

       NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

       NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

       NVIC_Init (&NVIC_InitStructure);

       TIM1_ClearITPendingBit (TIM1_FLAG_Update);   // Clear Interrupt

       TIM1_ITConfig (TIM1_FLAG_Update, ENABLE);    // Enable Interrupt

       TIM1_Cmd (ENABLE);                           // Enable Timer

    This next bit assumes a static variable called led_timer initialised to 0, that your LED is on port b and GPIO_LED is defined as the pin your LED is on.

    Find TIM1_UP_IRQHandler() in stm32f10x_it.c and put the following code there :-

    void TIM1_UP_IRQHandler(void)

    {

      TIM1_ClearITPendingBit (TIM1_FLAG_Update);

        led_timer=1-led_timer;

        if (led_timer)

         GPIO_ResetBits (GPIOB, GPIO_LED);

      else

         GPIO_SetBits (GPIOB, GPIO_LED);

    }

    That should get you a timer interrupt ticking. Play with the Period and Prescaler to get it running at the right speed.

    Sorry if it's a bit of a hack, I've taken it from bits of code I have and tied it together. Hopefully it will be enough to get you going.

    Cheers,

    lowpowermcu
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:11

    Hi ANN and andy,

    If you want to use TIM4 instead of TIM1, there is some differencies:

     - TIM4 is on APB1 and not on APB2

     - no repetition counter in TIM4 so no field  TIM_RepetitionCounter in timer struct

     - interrupt handler is ''TIM4_IRQHandler'' and not ''TIM1_UP_IRQHandler''

    That is what I have actually in mind.

    regards,

    MCU Lüfter

    lowpowermcu
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 14:11

    Hi ANN,

    I have looked for the site dedicated to STM32L family and I diidn't find eval board documentation neither ST library.

    I have found only reference manual ,datasheet and 2 application notes.

    Perhaps STM32L152-EVAL isn't from ST. could you trell us where to find it in Germany ?

    Thanks ANN,

    Herzlich,

    MCU Lüfter