Skip to main content
castillo
Associate II
Dec 29, 2010 10:52 AM UTC
Question

Timer in Slave Reset Mode: prescaler disabled?

Posted on December 29, 2010 at 11:52

Timer in Slave Reset Mode: prescaler disabled?

    This topic has been closed for replies.

    4 replies

    lowpowermcu
    Associate III
    May 17, 2011 12:19 PM UTC
    Posted on May 17, 2011 at 14:19

    Hi maverick,

    Can you give me the timer config to check it.

    Hope that I can help you.

    MCU Lüfter

    lowpowermcu
    Associate III
    May 17, 2011 12:19 PM UTC
    Posted on May 17, 2011 at 14:19

    Hi maverick,

    Where did you fid this ''Reference Manual says that when using slave mode, CK_CNT = CK_PSC.'' ?

    What I know is that counter prescaler can be used in slave and the capture prescaler can not be used

    so

      /* counter prescaler */

        TIM_TimeBaseStructure.TIM_Prescaler = the value of your choice but lower than 6535 ; /* Ignored in Slave Mode */ (I think that the comment is not correct)

    /* capture prescaler */

        TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; // can not be TIM_ICPSC_DIV2, TIM_ICPSC_DIV4 .......

    the prescaler is already set to 1 so if really the prescaler is ignored in slave mode, it should be 0 and not 1  .

    BTW, I can't find the software of the application note.

    Could you send it for me or tell me where I can find it (a link).

    MCU Lüfter

    castillo
    castilloAuthor
    Associate II
    May 17, 2011 12:19 PM UTC
    Posted on May 17, 2011 at 14:19

    Hello,

    The initialization code is basically the same than AN:

    void TIMEOUT_Init(TIM_TypeDef *tim) {

        TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

        TIM_ICInitTypeDef TIM_ICInitStructure;

        TIM_OCInitTypeDef TIM_OCInitStructure;

        if (tim == NULL) {

            return;

        }

        /* Stop timer */

        TIM_Cmd(tim, DISABLE);

        /* UEV disabled */

        TIM_UpdateDisableConfig(tim, ENABLE);

        /* Timer base configuration */

        TIM_TimeBaseStructure.TIM_Prescaler = 0x1; /* Ignored in Slave Mode */

        TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

        TIM_TimeBaseStructure.TIM_Period = 65535; /* Maximum period */

        TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;

        TIM_TimeBaseInit(tim, &TIM_TimeBaseStructure);

        /* Enable One-Pulse mode, so counter stops at UEV */

        TIM_SelectOnePulseMode(tim, TIM_OPMode_Single);

        /* Input Capture Configuration: Channel 1 */

        TIM_ICStructInit(&TIM_ICInitStructure);

        TIM_ICInitStructure.TIM_Channel = TIM_Channel_1;

        TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;

        TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

        TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;

        TIM_ICInitStructure.TIM_ICFilter = 0;

        TIM_ICInit(tim, &TIM_ICInitStructure);

        /* Output Compare  Mode configuration: Channel2 */

        TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;

        TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Disable;

        TIM_OCInitStructure.TIM_Pulse = (uint16_t)0xFFFF; /* Timeout value */

        TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low;

        TIM_OC2Init(tim, &TIM_OCInitStructure);

        /* Timer Input trigger configuration: input connected to TI1 */

        TIM_SelectInputTrigger(tim, TIM_TS_TI1FP1);

        /* Timer configuration in slave reset mode where the timer counter is

           re-initialized in response to rising edges on the input capture (TI1) */

        TIM_SelectSlaveMode(tim, TIM_SlaveMode_Reset);

        /* Global Interrupt mode */

        tim->CR1 &= (~TIM_CR1_URS);

        /* Update ARR, PSC and CCR shadow regs by setting UG bit in EGR reg */

        TIM_GenerateEvent(tim, TIM_EventSource_Update);

    }

    Interrupt handler starts the counter when the first byte is received (first rising edge in Rx input) until the counter matchs OC value. The problem is that TIM_Prescaler is ignored in slave mode (as mentioned in the reference manual), so counter frequency is too fast for UART common baudrates. If you could find a workaround to fix this, it will be really appreciated.

    Thank you.

    castillo
    castilloAuthor
    Associate II
    May 17, 2011 12:19 PM UTC
    Posted on May 17, 2011 at 14:19

    Hello!

    I'm really sorry for this very late answer, but I've been really busy with another proyect. The AN is here:

    http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/an3109.zip

    I will try your solution and let you know.

    Thank you!