Skip to main content
laurie
Associate II
February 17, 2012
Question

Timer in gated mode

  • February 17, 2012
  • 2 replies
  • 1011 views
Posted on February 17, 2012 at 12:46

I need to read from a zacwire device into the STM32.

I thought I could achieve this by using TIM2 setup in gated mode.

The idea was that I could then time the length of the start bit ( 1/2 bit length low pulse) and use that to sample subsequent bits.

I have PA.0 (TIM2_CH1) set as floating input.

I was expecting to see TIM2_CCR1 as the value of the capture caught in the interrupt but the interrupt is not called and CCR1 does not change when view with uVision.

This is what I have setup:

TIM_ICInitStructure.TIM_ICMode = TIM_ICMode_ICAP;

TIM_ICInitStructure.TIM_Channel = TIM_Channel_1;

TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling;

TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;

TIM_ICInitStructure.TIM_ICFilter = 0x0;

TIM_ICInit(TIM2, &TIM_ICInitStructure);

TIM_SelectInputTrigger(TIM2, TIM_TS_TI1FP1);

TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Gated);

TIM_TimeBaseStructure.TIM_Period = 0xFFFF;

TIM_TimeBaseStructure.TIM_Prescaler = 0;

TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseInit(TIM2, & TIM_TimeBaseStructure);

/* Enable the CC2 Interrupt Request */

TIM_ITConfig(TIM2, TIM_IT_CC1, ENABLE);

/* TIM enable counter */

NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQChannel;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = configLIBRARY_KERNEL_INTERRUPT_PRIORITY;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init( &NVIC_InitStructure );

TIM_Cmd(TIM2, ENABLE);

Nothing I've found has helped me.

What am I missing? ...Laurie:{)

#timer-gated
This topic has been closed for replies.

2 replies

esiqueira
Associate III
February 23, 2012
Posted on February 23, 2012 at 14:44

Do you have enabled

the device

?

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

laurie
laurieAuthor
Associate II
February 28, 2012
Posted on February 28, 2012 at 02:02

Hi Siqueira,

Thanks for the suggestion, but I have the clock enabled.

I've not been able to progress with it.           ...Laurie:{)