timer channels STM32F303x6/x8
Hi! Regarding the microcontroller STM32F303x6/x8.
I have to generate 4+4 PWM waveforms. Waveforms from 1 to 4 have the same frequency but each must have different duty cycle. The waveforms from 5 to 8 have same frequency (different from the first group) but each has different duty cycle. I want to use one timer for the first group. And another timer for the second group. The datasheet states "4 independent channels for output compare" in each chapter describing the timers. What does it mean? Are There 4 channels for each timer? or are there 4 channels for each group of timers (4 channels shared for TIM2/TIM3/TIM4 and other 4channels shared for TIM1/TIM8/TIM20)? or are there only 4 channels for all the timers of the microcontroller? thank you.