Skip to main content
Rogers.Gary
Senior II
February 3, 2015
Question

Timer Capture for frequencies < 100Hz

  • February 3, 2015
  • 12 replies
  • 2270 views
Posted on February 03, 2015 at 02:20

Hello,

I am endeavoring (as with every hair-pulling experience with the STM32F4) to measure/capture LOW frequency pulses. For this, I'm assuming I need to use a 32 bit timer: TIM2 or TIM5.

This is a bit of a dilemma since TIM2 or TIM5 do not have a capture compare. So how to measure low frequency pulses?

Thank you....

#stm32f4-timer-capture-compare
This topic has been closed for replies.

12 replies

Rogers.Gary
Senior II
February 4, 2015
Posted on February 04, 2015 at 01:04

Ok - I thought you were referring to something different than what was in the function pasted.

I'm actually using the function to read a signal that's more like a sine wave, periodic in nature. It seems to capture good, considering the signal. I may end up buffering through a Scmitt trigger to give it more of a pulse, but for now it should work.

I found that changing the filter from 0x0 to 0xf made some difference, depending on the amplitude of the signal. I'll need to read on that to see exactly what it does and what kind of signals it is designed for.

thanks clive1.

Rogers.Gary
Senior II
February 4, 2015
Posted on February 04, 2015 at 01:17

I checked the manual out. Looks like the filter might come in handy for what I'm doing.

I am transmitting a finite number of cycles at a given frequency, and it seems the filter can be programmed to ''validate'' after reaching the programmed number of captures - in powers of 2. A value of 0x3 = 2^3 = 8 cycles, which would be a good number to start with in my application. Awesome stuff.