Skip to main content
psandesh007
Associate II
June 24, 2013
Question

timer capture compare

  • June 24, 2013
  • 15 replies
  • 3037 views
Posted on June 24, 2013 at 15:22

Im going to capture simultaneously 4 input signals(same inputs for 4 channels) using Timer 8 by enabling all the interrupts in TIM->CCER register .. But it was not capturing correctly and im getting  channel number  2 and 4 continuously compared to 1 and 3 channels while im giving same frequency for all the channels..

please help me to solve this problem..
    This topic has been closed for replies.

    15 replies

    psandesh007
    Associate II
    July 1, 2013
    Posted on July 01, 2013 at 15:25

    Im still in problem to capture the accurate frequency of cascaded two timers please help me to overcome this problem ..

            ch4_CAP=TIM3->CCR1;

            ch4_CAP2=TIM1->CNT;

            if(ch4_CAP2>=ch4_CAP3)

            {

                gl31_captval_CH4=((65535*ch4_CAP2)+ch4_CAP)-((65535*ch4_CAP3)+ch4_CAP1);

            }

            else

            {

                   ch4_CAP3=65535-ch4_CAP3;

                gl31_captval_CH4=(65535*(ch4_CAP2+ch4_CAP3))+(ch4_CAP-ch4_CAP1);

            }

            ch4_CAP1=TIM3->CCR1;

            ch4_CAP3=TIM1->CNT;

    I tried in so many ways but still the frequency was fluctuating (all channels frequencies  are fluctuating at the same time)

    Tesla DeLorean
    Guru
    July 1, 2013
    Posted on July 01, 2013 at 17:13

    It's a bit of a mess, some of the logic/math is backward, and count should be 65536. This is compounded by a race condition because the high order counter isn't latched, but incremented by a free running counter.

    I would use the timer to get the low order precision, and use a high precision, high rate 32-bit counter to mark time and obtain the high order difference.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    July 1, 2013
    Posted on July 01, 2013 at 23:39

    This is a blind implementation, as there's no code framework. Assumes TIM3 is slaved off TIM1, and Period=65535; (N-1)

    uint32_t captured[6];
    void TIM3_IRQHandler(void)
    {
    uint32_t timebase;
    uint16_t timehigh1, timehigh2, timelow;
    do
    {
    timehigh1 = TIM3->CNT; // High order, 1/65536th rate on slave
    timelow = TIM1->CNT; // Low order, high rate, will change by a dozen or so ticks
    timehigh2 = TIM3->CNT; // Catch rollover, if it occurred
    }
    while(timehigh1 != timehigh2); // Overflowed, try over, perhaps 1 additional iteration
    timebase = ((uint32_t)timehigh1 << 
    16
    ) | (uint32_t)timelow;
    // Then for each channel
    if (TIM_GetITStatus(TIM3, TIM_IT_CC1) == SET)
    {
    uint16_t 
    ccr
    = 
    TIM3
    ->CCR1; // note use of local/static with same names to limit typos
    static uint16_t ccrlast;
    static uint32_t timelast;
    uint32_t timedelta, ccrdelta;
    /* Clear TIM3 Capture compare interrupt pending bit */
    TIM_ClearITPendingBit(TIM3, TIM_IT_CC1);
    timedelta = (timebase - timelast) >> 16; // error perhaps a few 100 cycles, but we truncate by 65536, so just rounding noise
    timelast = timebase; 
    ccrdelta = (uint32_t)(ccr - ccrlast); // implicitly & 0xFFFF 
    ccrlast = ccr;
    captured[4] = ccrdelta + (timedelta << 16); // Use an array! inherit channel 4 designation
    } // sourcer32@gmail.com
    
    // ..
    }

    Now there is at least one flaw in this method, if the period of the input signal is close to the 16-bit overflow it might underestimate. One way of addressing this would be to compute a rough delta, and compare that to the fine computation. If the rough estimate was around 60000 cycles more, then you have identified a cycle slip in the high order and would correct the fine computation with a += 655
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    psandesh007
    Associate II
    July 3, 2013
    Posted on July 03, 2013 at 07:00

    Thank you clive im trying still.

    psandesh007
    Associate II
    July 9, 2013
    Posted on July 09, 2013 at 14:34

    I got it. i was not given the frequency for the slave timer .. Now it is cleared.. thank you..