Timer adapted to HAL Standards from previous code
Hi,
I'm trying to adapt the following code, from previous versions, to HAL Cubemx standards :
void TIM1_CC_IRQHandler(void)
{
uint32_t break_time, mab_time;
TIM_ClearITPendingBit(TIM1, TIM_IT_CC1);
break_time = TIM_GetCapture2(TIM1);
mab_time = TIM_GetCapture1(TIM1) - break_time;
/* use some tolerance for times */
if (break_time > 80 && break_time < 10e3 && mab_time > 8) {
start_flag = 1;
TIM_ITConfig(TIM1, TIM_IT_CC1, DISABLE);
}
}
So far, the functions on the timer are not accepted on HAL, and I couldn't see anything about TIM_ITConfig on the documentation
Do you have any idea?
Thank you in advance
ip