Skip to main content
Tommino
Associate III
March 10, 2022
Solved

Timer 2 clocks timer 5 in Nucleo L476RG

Hello,

I would like to make timer 2 compare event in channel 1 to clock timer 5. Timer 2 compare events also sends DMA request and timer 5 is also used to output a PWM waveform.

Here you can find the Init function that I wrote and the main code. At the end something is not working because I can't see any waveform at PAO (the one supposed to output the PWM). I double checked the Timer registers and they seem fine to me. Can you help me in finding the errors? I am not able to undesrtand wheter the problem is on the TIM2 or TIM5 (both the timer synchronization part and the GPIO configuration)

I shared only the relvant code for the two timers and removed

 
 
 
 
 
 
// timer2 initialization
void TIM2Init (void){
	 // Enable the timer clock
	 RCC->APB1ENR1 |= (1<<0); // Enable the tim2 clock writing 1 in bit 0
	 // Set the prescaler and the ARR to set the frequency of the sinewave
	 TIM2 -> PSC = 79; // 80 MHz/80= 1MHz clock --> 1us count
	 TIM2-> ARR = 5; // ARR value uguale a CCR va bene? o deve essere più alto?
	 TIM2 -> CCR1= 5; // ogni volta che c'è il compare riparte da zero
	 TIM2 -> CCR2= 5; // ogni volta che c'è il compare riparte da zero
	 TIM2 -> CR2 |= (1<<6)|(0<<5)|(0<<4); // Master mode selection Bits 6:4 MMS[2:0]=100
	 // TIM2 -> SMCR |= (1<<7); (TBC)
	 TIM2 -> EGR |= (1<<1) | (1<<2); // compare event generation enabled 
	 TIM2 -> DIER |= (1<<9); // Enable the DMA request when compare 1
	 TIM2 -> DIER |= (1<<10); // Enable the DMA request when compare 2
}
 
// Tim5 is the slave timer clocked by tim 2 PWM Mode 
void TIM5Init (void){
	 // Enable the timer clock (not necessary?)
	 //RCC->APB1ENR1 |= (1<<3); // Enable the tim5 clock writing 1 in bit 3
	 // Set the period (ARR) and duty (CCR1): Frequency TimClock/ ARR. Duty cycle set by CCR/ARR
	 TIM5-> ARR = 100; // ARR value --> period equal to the number of samples of the sinusoidal waveform
	 TIM5-> CCR1= 50;
	 // set the slave mode: the clock is the compare event of tim2_ch1
	 TIM5 -> SMCR|= (1<<0)|(1<<1)|(1<<2); // SMS=111 external clock mode 1 and TS=000 internal trigger 0
	 // set the PWM mode
	 TIM5 -> CCMR1 |= (0<<0); // to set the output compare mode
	 TIM5 -> CCMR1 |= (1<<3); // OC1PE bit to enable the preload register
	 TIM5 -> CCMR1 |= (6<<4); // OC1M bits to set the PWM mode in ch1
	 TIM5 -> CR1 |= (1<<7); // ARPE BIT:ARR register is buffered
	 //TIM5-> EGR |= (1<<1); // Enable the compare event
	 TIM5 -> CCER |= (0<<1); // CC1P bits to set the polarity (write 0 in bit 1 to have active high)
	 TIM5-> CCER |= (1<<0); // output on the corresponding output pin enable
	 // Enable the GPIOA Clock
	 RCC-> AHB2ENR |= (1<<0); // Enable the GPIOA clock writing 1 in bit 0
	 // Configure the GPIO (PAO AlternateFunction2) to output the PWM
	 GPIOA -> MODER |= (1<<1); // PAO configured as alternate function
	 GPIOA -> AFR[0] |= (1<<1); // Set alternate Function 2 (AFR[0] is called GPIOx_AFRL in the manual)
	 GPIOA -> OTYPER |= (0<<0); // output as push-pull
	 GPIOA -> PUPDR |= (0<<0); // No pullup or pulldown
	 GPIOA -> OSPEEDR |= (1<<0); // Medium Speed
	 //
}
 
 
 
 
 
 //
 
 
/* USER CODE END 0 */
 
 
int main(void)
{
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SPI1_Init();
 MX_SPI2_Init();
 /* USER CODE BEGIN 2 */
 TIM2Init();
 TIM5Init();
 DMA1_Init();
 
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 
 
 TIM2 -> CR1|= (1<<0); // Enable Timer2
 TIM5 -> CR1|= (1<<0); // Enable Timer5 for PWM
 
 
 
 
 
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 10;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief SPI1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_SPI1_Init(void)
{
 
 /* USER CODE BEGIN SPI1_Init 0 */
 
 /* USER CODE END SPI1_Init 0 */
 
 /* USER CODE BEGIN SPI1_Init 1 */
 
 /* USER CODE END SPI1_Init 1 */
 /* SPI1 parameter configuration*/
 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_MASTER;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES;
 hspi1.Init.DataSize = SPI_DATASIZE_16BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi1.Init.NSS = SPI_NSS_HARD_OUTPUT;
 hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 7;
 hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI1_Init 2 */
 
 /* USER CODE END SPI1_Init 2 */
 
}
 
/**
 * @brief SPI2 Initialization Function
 * @param None
 * @retval None
 */
static void MX_SPI2_Init(void)
{
 
 /* USER CODE BEGIN SPI2_Init 0 */
 
 /* USER CODE END SPI2_Init 0 */
 
 /* USER CODE BEGIN SPI2_Init 1 */
 
 /* USER CODE END SPI2_Init 1 */
 /* SPI2 parameter configuration*/
 hspi2.Instance = SPI2;
 hspi2.Init.Mode = SPI_MODE_MASTER;
 hspi2.Init.Direction = SPI_DIRECTION_2LINES;
 hspi2.Init.DataSize = SPI_DATASIZE_16BIT;
 hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi2.Init.NSS = SPI_NSS_HARD_OUTPUT;
 hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
 hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi2.Init.CRCPolynomial = 7;
 hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
 if (HAL_SPI_Init(&hspi2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN SPI2_Init 2 */
 
 /* USER CODE END SPI2_Init 2 */
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
 
 /*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */
 GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This topic has been closed for replies.
Tommino
TomminoBest answer
Associate III
March 10, 2022

Solved :)

Timer 5 shall be enabled before tim2

1 reply

Tommino
TomminoAuthorBest answer
Associate III
March 10, 2022

Solved :)

Timer 5 shall be enabled before tim2