Skip to main content
PGood.1
Associate III
December 16, 2020
Question

timer 16 interupt not trigering on a stm32L432

Im migrating the code from a stm32L031 to a stm32L432 and the timer interupt isnt triggering Ive set the LED to toggle in the CaptureCallback. This code works on a L031 using timer22. Clearly Im missing something obvious;

void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)

{

 uint8_t byteindex;

 uint8_t byteoffset;

 HAL_GPIO_TogglePin(LD3_GPIO_Port, LD3_Pin);

 if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)

 {

  new_cap = htim16.Instance->CCR1;

  if (new_cap > old_cap){

  time = new_cap - old_cap;

  }else{

  time = 65535 - old_cap + new_cap;

  }

  older_cap=old_cap;

  old_cap = new_cap;

}

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};

 /** Configure LSE Drive Capability

 */

 HAL_PWR_EnableBkUpAccess();

 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

 /** Initializes the RCC Oscillators according to the specified parameters

 * in the RCC_OscInitTypeDef structure.

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_LSE

               |RCC_OSCILLATORTYPE_MSI;

 RCC_OscInitStruct.LSEState = RCC_LSE_ON;

 RCC_OscInitStruct.LSIState = RCC_LSI_ON;

 RCC_OscInitStruct.MSIState = RCC_MSI_ON;

 RCC_OscInitStruct.MSICalibrationValue = 0;

 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;

 RCC_OscInitStruct.PLL.PLLM = 1;

 RCC_OscInitStruct.PLL.PLLN = 16;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;

 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;

 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the CPU, AHB and APB buses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)

 {

  Error_Handler();

 }

 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;

 PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;

 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure the main internal regulator output voltage

 */

 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)

 {

  Error_Handler();

 }

 /** Enable MSI Auto calibration

 */

 HAL_RCCEx_EnableMSIPLLMode();

}

/**

 * @brief TIM16 Initialization Function

 * @param None

 * @retval None

 */

static void MX_TIM16_Init(void)

{

 /* USER CODE BEGIN TIM16_Init 0 */

 /* USER CODE END TIM16_Init 0 */

 TIM_IC_InitTypeDef sConfigIC = {0};

 /* USER CODE BEGIN TIM16_Init 1 */

 /* USER CODE END TIM16_Init 1 */

 htim16.Instance = TIM16;

 htim16.Init.Prescaler = 32;

 htim16.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim16.Init.Period = 65535;

 htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 htim16.Init.RepetitionCounter = 0;

 htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

 if (HAL_TIM_Base_Init(&htim16) != HAL_OK)

 {

  Error_Handler();

 }

 if (HAL_TIM_IC_Init(&htim16) != HAL_OK)

 {

  Error_Handler();

 }

 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;

 sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;

 sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;

 sConfigIC.ICFilter = 0;

 if (HAL_TIM_IC_ConfigChannel(&htim16, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN TIM16_Init 2 */

 /* USER CODE END TIM16_Init 2 */

}

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
December 16, 2020

Not ALL the related code end-to-end.

Check the IRQHandler, the linkage (that the linker actually bound the code), and NVIC enabling..

TIM1_UP_TIM16_IRQHandler

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PGood.1
PGood.1Author
Associate III
December 23, 2020

Got the IRQ handler going by adding HAL_TIM_IC_Start_IT(&htim16, TIM_CHANNEL_1); in the main() function