Skip to main content
vinay bhat
Associate
Dec 15, 2018 10:32 AM UTC
Solved

Time Triggered CAN communication support

I am currently in a process of selecting micro controller for my project. Basically i need TTCAN support and i have STM32F746G Disco board with me. Now as per the ST reference manual i see that this is supported. Now my questions are...

  1. Is there any reference available for TTCAN implementation?
  2. If the HW supports TTCAN, can i completely rely on HW module?

ex: who will generate reference message(defined in TTCAN spec) ? HW or my SW?

3.Can i make STM32F746G as master of my TTCAN cluster ?

Unfortunately i could not find much details in the internet and the ST reference manual. If anybody has prior knowledge of working on this topic please do respond.

Thanks :| !!

This topic has been closed for replies.
Uwe Bonnes
Uwe BonnesBest answer
Chief
Dec 15, 2018 10:59 AM UTC

Read the errata sheets. Since the first STM32 up to the STM32F76 there is an item:

"BxCAN time triggered mode not supported . "

5 replies

Uwe Bonnes
Uwe BonnesBest answer
Chief
Dec 15, 2018 10:59 AM UTC

Read the errata sheets. Since the first STM32 up to the STM32F76 there is an item:

"BxCAN time triggered mode not supported . "

vinay bhat
Associate
Dec 15, 2018 11:07 AM UTC

Oh yes. I verified it. Thanks for saving my time and effort. BTW, is there any other MCU in ST which support TTCAN ?

Uwe Bonnes
Chief
Dec 15, 2018 11:40 AM UTC
vinay bhat
Associate
Dec 17, 2018 4:23 PM UTC

Unfortunately, FDCAN does'nt serve the purpose !!.

do you know if ST has fixed this errata in subsequent HW releases? Ex: STM32F76. I cannot find any official Errata sheet for STM32F76x in ST websites.

kacem.halim
Visitor II
Feb 15, 2019 8:02 AM UTC

CAN FD implemented in new STM32 MCU can be used as classic CAN, based on that you can use TTCAN.