Skip to main content
Were-Rabbit
Associate II
July 19, 2010
Question

TIM4 PWM Out

  • July 19, 2010
  • 4 replies
  • 870 views
Posted on July 19, 2010 at 13:25

TIM4 PWM Out

    This topic has been closed for replies.

    4 replies

    swhite2
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:59

    You only need that for Timers 1 and 8 (if present). You do, however, need to enable the GPIO port, alternate function and timer clocks though.

    John F.
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:59

    This worked for Timer1. Do you need to use function, TIM_CtrlPWMOutputs(TIMx, ENABLE) ?

    John F.

    #include ''stm32f10x.h''

    void RCC_Configuration(void);

    void GPIO_Configuration(void);

    void Timer1_Configuration(void);

    //note with SYSCLK_FREQ_72MHz defined, PCLK1 = 36MHz and PCLK2 = 72MHz

    uint16_t CCR1_Val = 1000; //1500 = 1.5ms (1000 = 1ms, 2000 = 2ms);

    int main(void)

    {

      RCC_Configuration();

      GPIO_Configuration();

      Timer1_Configuration();

      while(1)

      {

        GPIO_WriteBit(GPIOB, GPIO_Pin_0, Bit_SET);

        GPIO_WriteBit(GPIOB, GPIO_Pin_0, Bit_RESET);

      }

    }

    void RCC_Configuration(void)

    {

      //Setup the microcontroller system. Initialize the Embedded Flash Interface, 

      //initialize the PLL and update the SystemFrequency variable.

      SystemInit();

     

      // Enable GPIOB, AFIO and Timer1 clocks

      RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO | RCC_APB2Periph_TIM1, ENABLE);

    }

    void GPIO_Configuration(void)

    {

      GPIO_InitTypeDef GPIO_InitStructure;

      //partial remap of Timer1

      GPIO_PinRemapConfig(GPIO_PartialRemap_TIM1, ENABLE);

      //GPIOB Configuration: TIM1 channel 2N as alternate function push-pull

      GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_0;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

      GPIO_Init(GPIOB, &GPIO_InitStructure);

    }

    void Timer1_Configuration(void)

    {

      //Timer1 is clocked by PCLK2 = 72MHz

      TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

      TIM_OCInitTypeDef  TIM_OCInitStructure;

      TIM_DeInit(TIM1);

      //Time base configuration

      TIM_TimeBaseStructure.TIM_Prescaler = 71; //clocked at 72MHz / 72 = 1MHz

      TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

      TIM_TimeBaseStructure.TIM_Period = 19999; //period = (72MHz / 72) / 20000 = 50Hz (20ms period)

      TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;

      TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);

      /* Channel 1 Configuration in PWM mode */

      TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;

      TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;

      TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable;

      TIM_OCInitStructure.TIM_Pulse = CCR1_Val;

      TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;

      TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;

      TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;

     

      TIM_OC2Init(TIM1, &TIM_OCInitStructure);

      TIM_OC2PreloadConfig(TIM1, TIM_OCPreload_Enable);

      TIM_CtrlPWMOutputs(TIM1, ENABLE);

      //TIM1 enable counter

      TIM_Cmd(TIM1, ENABLE);

    }

    cris
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:59

    Hello Mr. John F.

    Im using the same code to generate a PWM that you posted here but i can`t get any signal.

    I want to use it to control a RGB LED so i changed the GPIO configuration but i cant get any signal...

    is there anything else i need to do it?

    Thank you

    Were-Rabbit
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:59

    Thank You, PWM1 is working