Question
TIM2 Interrupt issue
Posted on December 11, 2012 at 09:30
Hello all experts,
I configured the TIM2 in my STM32F4 discovery board such that it gives me interrupts every 50ms. The code is as follows. ********************************* void TIM2_IRQHandler(void) { if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET) { TIM_ClearITPendingBit(TIM2, TIM_IT_Update); GPIO_ToggleBits(GPIOA, GPIO_Pin_5); }} ********************************* void INTTIM_Config(uint16_t numOfMilleseconds) { NVIC_InitTypeDef NVIC_InitStructure; /* Enable the TIM2 gloabal Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* TIM2 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = (500*numOfMilleseconds) - 1; // 1 MHz down to 1 KHz (1 ms) //TIM_TimeBaseStructure.TIM_Prescaler = 84 - 1; // 24 MHz Clock down to 1 MHz (adjust per your clock) TIM_TimeBaseStructure.TIM_Prescaler = 168-1; //168MHz Clock should be down to 1MHz TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); /* TIM IT enable */ TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); /* TIM2 enable counter */ TIM_Cmd(TIM2, ENABLE); } ******************************************* int main(void) { GPIO_config(); INTTIM_Config(50); while (1) { } } **************************************************** - I'm checking the PA5 signal with the oscilloscope and what I expect is to toggle the signal in each 50ms interval. - My problem is when I check this with the scope, I see that when I run TIM_Cmd(TIM2, ENABLE); command, program jumps to the interrupt routine. - As a summary, interrupt routine is executed when I enable the time. Can someone please help me with this issue. Thank you for spending your valuable time. Regards, Thilina #adc-and-tim2-interrupt. #discovery-board