Skip to main content
pawelcit
Associate
Dec 28, 2011 1:30 AM UTC
Question

TIM1 configuration and it's behavior

Posted on December 28, 2011 at 02:30

Hi, first of all sorry for my english but I hope you will understand me.

Here is a TIM1 configuration form DSO nano project. I've rewrited it to more readable format:

TIM1->PSC = 30;

TIM1->ARR = 35;

TIM1->CCR1 = (35+1)/2;

TIM1->CR1 = TIM_CR1_DIR | TIM_CR1_URS | TIM_CR1_ARPE;

TIM1->RCR = 0x0000;

TIM1->CCER = TIM_CCER_CC1E;

TIM1->CCMR1 = TIM_CCMR1_OC1FE | TIM_CCMR1_OC1PE | TIM_CCMR1_OC1M;

TIM1->BDTR = TIM_BDTR_MOE;

TIM1->DIER = TIM_DIER_CC1DE |TIM_DIER_UDE | TIM_DIER_TDE;

TIM1->CR1 = TIM_CR1_CEN;

Can somebody explain me how this configuration behave? Am I correct if I think the period of occuring events is (PSC+1)*(ACC+1)/72MHz ? (does the TIM1->CCR1 = (35+1)/2; have any meaning?) How works bits TDE and UDE?

I take a simple experiment with this configuration with set bits TDE  UDE and without them but I dont see any difference (of course in DMA usage).
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Dec 28, 2011 5:16 PM UTC
    Posted on December 28, 2011 at 18:16

    Pretty limited desire to decipher bit level TIM configurations.

    The value of ARR suggests a frequency of about 64.516 KHz.

    The computation for CCR1 suggests a desire for a 50/50 duty cycle.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    pawelcit
    pawelcitAuthor
    Associate
    Dec 28, 2011 5:52 PM UTC
    Posted on December 28, 2011 at 18:52

    Thank You for reply. This configuration in general was created to trigger ADC by timer's events. Does the duty cycle (in this case 50%) have any  effect to the frequency of events? What would be in case of ex. 10% duty cycle?

    What do CC1DE, UDE and TDE bits do

    practically

     ?