Skip to main content
JMED.1
Visitor II
April 1, 2020
Question

TIM1: can I change Dead Time on the fly ?

  • April 1, 2020
  • 1 reply
  • 623 views

I need to change the dead time of the TIM1 complementary outputs cycle by cycle. What is the behavior if I just overwrite the DTG[7:0] value during a cycle: does it change the actual dead time of the next cycle? or the current?

Thank you in advance.

This topic has been closed for replies.

1 reply

Uwe Bonnes
Chief
April 2, 2020

As long as no locking is set, the reference manual implies that you can change the DTR value.and that should have an effect!