Associate II
October 5, 2013
Question
TIM_OCMode_Toggle PWM Duty Controll
- October 5, 2013
- 15 replies
- 3784 views
Posted on October 05, 2013 at 08:36
I'm an absolutely beginner in microcontrollers.
I want to create a PWM signal wave signal to drive main power switch at 100Khz TIM1CH1&TIM1CH1N of STM32F103VC. I change duty (CCR1_Val) but the duty stay same at 50%. Can anybody tell me what I'm doing wrong? Thank You Photo to Attachments vu16 CCR1_Val = 90 ; TIM_DeInit(TIM1); /* Time Base configuration */ TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_Period = 360 - 1 ; // 72 MHz / 360 = 200 kHz TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1,&TIM_TimeBaseStructure); /* Channel 1, 2,3 and 4 Configuration in PWM mode */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle ; TIM_OCMode_PWM1 TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Enable; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_Low; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCNPolarity_Low; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set; TIM_OCInitStructure.TIM_OCIdleState = TIM_OCNIdleState_Set; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; // 25% TIM_OC1Init(TIM1,&TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM1, TIM_OCPreload_Enable); /* TIM1 counter enable */ TIM_Cmd(TIM1,ENABLE); /* Main Output Enable */ TIM_CtrlPWMOutputs(TIM1,ENABLE);