Skip to main content
TDJ
Senior III
Sep 6, 2024 5:14 PM UTC
Question

ThreadX status and future

Hi All,

Not so long ago ST has selected Microsoft ThreadX as one of its its strategic technologies.
In my opinion it is a very good RTOS. The problem is that it was supported by Microsoft only, no other community project integrates with it, e.g. mcuboot etc. It is almost like ThreadX does not exist.
Now, Microsoft ThreadX is Eclipse-ThreadX. It is open-source, MIT licensed but last Github commit was made 6 months ago. The latest version is 6.4.1 while ST is still stacked with version 6.2.0.

No significant ST 's commitment is visible. It does not look good - regretfully, I need to say.

Am I missing something?

I need to decide whether I should use it in my project or abandon while I still have a choice.

This topic has been closed for replies.

18 replies

Visitor II
Sep 6, 2024 5:32 PM UTC

If your project has a long timeline and requires extensive community support and ecosystem integration, it will be wise to consider alternatives like FreeRTOS or Zephyr.

TDJ
TDJAuthor
Senior III
Sep 6, 2024 6:25 PM UTC

@liaifat85 That is what I start to think. There are no signs ST wants to pick this ball up, probably eventually ST will drop ThreadX and go back to FreeRTOS or switch to Zephyr, unless something more exotic will gain sympathy of some VP detached from reality.

Pavel A.
Sep 6, 2024 10:07 PM UTC

Unfortunately this is "the Microsoft Way". Most of their affairs with acquired projects or companies... Anybody remembers what they did with Nokia? Skype?  Now their darling is Rust. 

So the status: free cheese is not forever. Future: expect more hard work.

TDJ
TDJAuthor
Senior III
Sep 7, 2024 7:51 AM UTC

@Pavel A. Particularly painful was how Microsoft cancelled Silverlight after when Miguel de Icaza demonstrated Mono/Moonlight on Android. Ofc, the official reason was different but I know for certain. I lost startup company, more than a year of work and considerable money and will never trust them again.

Pavel A.
Sep 7, 2024 12:55 PM UTC

@TDJ Yes there were the times. Churn and huge waste of resources is unavoidable in this industry. Been in the WiMax project. But guess what - my current job is "powered by" Microsoft ))

BarryWhit
Lead
Sep 7, 2024 1:52 AM UTC

You will find plenty of dysfunction on the zephyr repo as well. and there's the epic malloc bug saga for FreeRTOS that took place on this forum, and is still in a murky state. 

 

No free lunch.

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
TDJ
TDJAuthor
Senior III
Sep 7, 2024 7:54 AM UTC

@BarryWhit This is why I hesitate. ThreadX appears to be stable, well-thought, consistent, well tested and well certified. I mean, quite solid piece of software. Too bad probably it is going to be abandoned.
I am on the fence and ST is silent.

Tesla DeLorean
Guru
Sep 7, 2024 3:58 PM UTC

ST isn't making a contractual commitment to ANY of this. You get to own your own decisions and choices.

Microsoft is a sh**ty partner, have been for decades, I wouldn't tie any of my business to them, ever.

Provided there's not bit rot, there's no reason you can't adopt a current release, and maintain and patch that yourself. We're not building Adobe Flash

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TDJ
TDJAuthor
Senior III
Sep 7, 2024 6:55 PM UTC

@Tesla DeLorean Exactly, ThreadX is no longer Microsoft and it is MIT licensed.
RTOS does not need to be the best. I do not work for SpaceX (yet). It just needs to be good enough.
Thank you for your input.

TDJ
TDJAuthor
Senior III
Sep 11, 2024 12:40 PM UTC

One more thought. The problem with ST, as I see it, is that as much as possible it tries to remain hardware company and maintain very minimum software it exclusively owns like CubeXX, TouchGFX etc. In some ways, maturity-wise ST is where Microsoft used to be during Steve Ballmer era.
The same time competition truly engages in community projects like mcuboot, trustedfirmware or lvgl where ST's presence is at best only pretended. ThreadX seems to fall into this pattern. Probably it was selected in the first place mainly because competitors could not offer it free. Since solutions we build consist of both hardware and software and time-to-market matters a lot, ST, although makes excellent hardware, to me by no means is a clear winner because competitors provide much more help with software.

Pavel A.
Sep 11, 2024 1:14 PM UTC

> because competitors provide much more help with software.

Really?

Andrew Neil
Super User
Sep 11, 2024 1:50 PM UTC

It's all just 3rd-party software - you don't have to rely on ST for any of it ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
Sep 11, 2024 1:58 PM UTC

@Andrew Neil Developing for graphic hardware depends on support and documentation of the vendor. For example new graphic controllers of H5 and U5 (?).  Even situation with USB and Ethernet is far from great (well, 3rd party IPs...). But are competitors much better?

Andrew Neil
Super User
Sep 11, 2024 2:04 PM UTC

@Pavel A. wrote:

 are competitors much better?


I think not.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDJ
TDJAuthor
Senior III
Sep 11, 2024 3:04 PM UTC

@Andrew Neil, @Pavel A. That depends on a particular area, project and expectations but if competitors were much butter, I would not be here and ST board would hold emergency meetings because of stocks falling down sharply. But I am neither ST VP nor stake holder and as an engineer I often have reasons to be unhappy. ThreadX uncertain future and U5 GPU2D docs are just two of them.