There seem to be a mismatch in the STM32H747 documentation: The 176 pin version should have an VDDDSI pin, but it's missing in the pin definition and in the pinout. Is it a typo?
According to the STM32H747xI/G datasheet, the STM32H747IG has a VCAPDSI pin, but no VDDDSI pin at all.
I'm sure i get something wrong here, because without VDDDSI pin, the VCAPDSI pin would be a miraculous source of energy! ;)
But seriously: do i have to connect an external LDO to the VDD12DSI pins? Or does the DSI regulator get its energy from an undocumented internal power routing in the 176 pin version?
Thanks a lot in advance!
Al
BTW: the pins 158 and 159 are swapped in the pinout (STM32H747xI/G datasheet)!