Skip to main content
Associate
Jul 20, 2026 7:44 AM UTC
Solved

There is a significant difference in current consumption between STOP mode and STANDBY mode on the STM32L031.

I built a low-power board using an STM32L031. The code I use to enter STOP mode and STANDBY mode is shown below.

In STANDBY mode, the board consumes about 2 µA. However, in STOP mode, it consumes about 90 µA, and I am not sure why there is such a large difference.

The circuit only consists of the STM32L031 and the power supply section. Could there be a problem with my code? Why is the current consumption so much higher in STOP mode than in STANDBY mode?

 

void EnterStopMode(void)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_2);

HAL_NVIC_ClearPendingIRQ(EXTI2_3_IRQn);

HAL_SuspendTick();

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

SystemClock_Config();

HAL_ResumeTick();
}



void EnterStandbyMode(void)
{
__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

HAL_PWR_EnterSTANDBYMode();
}
Gyessine
GyessineBest answer
ST Technical Moderator
Jul 20, 2026 9:26 AM UTC

Hello ​@eunoia 
It’s mentioned in the readme of the firmware example that you should disconnect PA12 pin from GND, when removed I managed to get few microamperes as consumption
I think I also should mention that I got the 85ua consumption (very close to yours) when i didn’t disconnect PA12 from GND pin
so are you sure that your PA12 pin is not connected to ground
I mean the experiments favours this hypothesis.
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Gyessine
GyessineBest answer
ST Technical Moderator
Jul 20, 2026 9:26 AM UTC

Hello ​@eunoia 
It’s mentioned in the readme of the firmware example that you should disconnect PA12 pin from GND, when removed I managed to get few microamperes as consumption
I think I also should mention that I got the 85ua consumption (very close to yours) when i didn’t disconnect PA12 from GND pin
so are you sure that your PA12 pin is not connected to ground
I mean the experiments favours this hypothesis.
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Gyessine
ST Technical Moderator
Sep 25, 2026 2:15 PM UTC

Hello ​@eunoia 
Any updates
is your issue solved?
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.