Skip to main content
Patrick Morwald
Associate III
March 19, 2018
Question

There are no instructions for calibrating ADC in STM32F407

  • March 19, 2018
  • 3 replies
  • 2810 views
Posted on March 19, 2018 at 16:15

Hi, 

after googling around a while and reading the STM32 manual section for the ADC, i am frustrated about the lack of such a section in the manual.

So how IS the ADC in the STM32F4 actually calibrated??

EDIT:

I found this thread: 

https://community.st.com/0D50X00009XkYIWSA3

 

However, if i do so on my STM32F407VGT (Discovery Board), i dont have a VREFINT_CAL value.

Should i just measure VREFINT on Channel 17 of the ADC and assume this is exactly 1.25 V?

Thanks,

Patrick

#stm32f4 #adc #adc-calibration
This topic has been closed for replies.

3 replies

AvaTar
Senior III
March 19, 2018
Posted on March 19, 2018 at 16:40

I might want to check the RM, but I faintly remember the ADC does the calibration automatically.

Or the ADC code in the SPL said so ...

Patrick Morwald
Associate III
March 19, 2018
Posted on March 19, 2018 at 16:47

Well, that would be OK for me if thats reliable. At least there are no library functions for calibration in my SDK...

STOne-32
ST Technical Moderator
March 19, 2018
Posted on March 19, 2018 at 17:45

Dear @Patrick

There is no hardware ADC calibration for our STM32F4, it is self-calibrated upon reset and once ADC is activated, However, I do not recommend to varies VDDA/ VREF+  voltage once ADC is activated, you should always keep them stable when it is active, else re-enable it again.  

For other STM32F1 as example, the calibration is able to compensate the Offset and you can do it from time to time when temperature change or VREF+  voltage Change.

Cheers,

STOne-32