Skip to main content
Associate II
July 10, 2024
Question

The program cannot start after commenting out a line of code

The main function code is as follows:

 

 

while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 loop_cnt++;

 //HAL_GPIO_TogglePin(LED_GPIO_Port,LED_Pin);
 if(13 == ((loop_cnt >> 4) & 0x0f))
 HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_RESET);
 else if (15 == ((loop_cnt >> 4) & 0x0f))
 HAL_GPIO_WritePin(LED_GPIO_Port, LED_Pin, GPIO_PIN_SET);
		
 HAL_IWDG_Refresh(&hiwdg);

 if(HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_13))
 {
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_6, GPIO_PIN_RESET);
 }
 else
 {
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_6, GPIO_PIN_SET);
 }

 //print_log("w5500 link STA %d\r\n", (Read_W5500_1Byte(PHYCFGR)&LINK));
 #if 1

 if((getPHYCFGR() & 0x01) != link_state)
 {
 link_state = (getPHYCFGR() & 0x01);

 if((getPHYCFGR() & 0x01) == 0)
 {
 beep_voice(1, 200);
 close(2);
 S_State[2] = 0;
 close(3);
 S_State[3] = 0;
 close(4);
 S_State[4] = 0;
 close(5);
 S_State[5] = 0;
 }
 else
 {
 beep_voice(2, 50);
 print_log("w5500 link\r\n");
 }
 }
		else if(memcmp(gSystemParam.deviceIp, gSystemParam.gateway, 3) == 0) // check gateway
 {
 //tmpTciks = g64msTicks;
 // handle webserver
 do_http(0);
 //print_log("do_http %lld\r\n", g64msTicks - tmpTciks);

 //tmpTciks = g64msTicks;
 // handle NTP services
 //ntpServices();
 //print_log("ntpServices %lld\r\n", g64msTicks - tmpTciks);

 //tmpTciks = g64msTicks;
 netAppServices();
 //read_net_app();
 //print_log("netAppServices %lld\r\n", g64msTicks - tmpTciks);
 }

 // handle uart message, include uart1 uart2 uart3
 cmdMachine();
		
 #endif

 }

 

 

After commenting out do_http(0); on line 54, the program cannot start. What is the problem?

The do_http function code is as follows:

 

char rx_buf[MAX_URI_SIZE] = {0};


void do_http(uint8_t sn)
{
 unsigned short len;

 st_http_request *http_request;
 memset(rx_buf,0x00,MAX_URI_SIZE);
 http_request = (st_http_request*)rx_buf;		// struct of http request 
 /* http service start */
 switch(getSn_SR(sn))
 {
 case SOCK_INIT:
 //listen(sn);
 break;
 case SOCK_LISTEN:
 break;
 case SOCK_ESTABLISHED:
 //case SOCK_CLOSE_WAIT:
 if(getSn_IR(sn) & Sn_IR_CON)
 {
 setSn_IR(sn, Sn_IR_CON);
 }
 if ((len = getSn_RX_RSR(sn)) > 0)		
 {
 len = recv(sn, (unsigned char*)http_request, len); 
 *(((unsigned char*)http_request)+len) = 0;
 //proc_http(sn, (unsigned char*)http_request); // request is processed
 disconnect(sn);
				//printf("SOCK_ESTABLISHED %04x\r\n", len);
 }
 break;
 case SOCK_CLOSE_WAIT: 
 if ((len = getSn_RX_RSR(sn)) > 0)
 {
 //printf("close wait: %d\r\n",len);
 len = recv(sn, (unsigned char*)http_request, len); 
 *(((unsigned char*)http_request)+len) = 0;
 //proc_http(sn, (unsigned char*)http_request); // request is processed
				//printf("SOCK_CLOSE_WAIT %04x\r\n", len);
 }
 disconnect(sn);
 break;
 case SOCK_CLOSED:
			len = gSystemParam.webServerPort[1];
			len *= 256;
			len += gSystemParam.webServerPort[0];
			socket(sn, Sn_MR_TCP, len, 0x00); /* reinitialize the socket */
 break;
 default:
 break;
 }// end of switch
}

 

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
July 10, 2024

I'd suppose it does start.

Replace rhe function call with a HAL_Delay(100) and see if it "works" again.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BOEINGNGAuthor
Associate II
July 10, 2024

No, it doesn't work. The segger RTT viewer doesn't has any output.

unsigned_char_array
Lead III
July 10, 2024

"the program cannot start"
What "program"? What do you mean by "start"?

A line in the "future" generally shouldn't affect a line before it.

Do you get compilation errors? Do you get errors when flashing? Do you get errors when debugging?
Or does the binary run, but doesn't do what you want it to do? If so, what is the desired/expected behavior vs what is the observed behavior? Does it hang in a loop? Hardfault errors?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
BOEINGNGAuthor
Associate II
July 10, 2024

Under normal circumstances, SEGGER RTT viewer has output and w5500 will connect to the server. However, after commenting out do_http(0), RTT viewer has no output and w5500 will not connect to the server. If you enter debug mode, you will find that the code is executing normally.

unsigned_char_array
Lead III
July 10, 2024

What server? I don't have my crystal ball at hand.
If the program doesn't do what you want when commenting out the line, then don't comment it out.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."