Skip to main content
Wei RP
Associate
Jun 14, 2018 5:23 PM UTC
Solved

the HAL has BUG of CAN drive on STM32F1?

Posted on June 14, 2018 at 19:23

Stm32F103 HAL_CAN_Transmit(&hcan,10) not working, always return HAL_TIMEOUT and HAL_ERROR, but when i use STD_Lib everything is good. So i think if the HAL has BUG of CAN on STM32F1?

Hello,

I'm trying to set up CAN on my STM32F103  to send a CAN message but I keep getting HAL_TIMEOUT error from the HAL_CAN_Transmit() function :

/* Check End of transmission flag */

while(!(__HAL_CAN_TRANSMIT_STATUS(hcan, transmitmailbox)))

{

/* Check for the Timeout */

   if(Timeout != HAL_MAX_DELAY)

   {

      if((Timeout == 0U) || ((HAL_GetTick()-tickstart) > Timeout))                           ///////here!!!!!!!!!!!!!

      {

         hcan->State = HAL_CAN_STATE_TIMEOUT;

         /* Cancel transmission */

         __HAL_CAN_CANCEL_TRANSMIT(hcan, transmitmailbox);

         /* Process unlocked */

         __HAL_UNLOCK(hcan);

         return HAL_TIMEOUT;

      }

   }

}

Here's my code:

/* Includes ------------------------------------------------------------------*/

&sharpinclude 'can.h'

&sharpinclude 'gpio.h'

/* USER CODE BEGIN 0 */

CanTxMsgTypeDef TxMessage;

CanRxMsgTypeDef RxMessage;

/* USER CODE END 0 */

CAN_HandleTypeDef hcan;

/* CAN init function */

void MX_CAN_Init(void)

{

hcan.Instance = CAN1;

hcan.pTxMsg = &TxMessage; //?????

hcan.pRxMsg = &RxMessage;

hcan.Init.Prescaler = 6;

hcan.Init.Mode = CAN_MODE_NORMAL;

hcan.Init.SJW = CAN_SJW_1TQ;

hcan.Init.BS1 = CAN_BS1_6TQ;

hcan.Init.BS2 = CAN_BS2_5TQ;

hcan.Init.TTCM = DISABLE;

hcan.Init.ABOM = DISABLE;

hcan.Init.AWUM = DISABLE;

hcan.Init.NART = ENABLE;

hcan.Init.RFLM = DISABLE;

hcan.Init.TXFP = DISABLE;

if (HAL_CAN_Init(&hcan) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

CAN_FilterConfTypeDef sFilterConfig;

//

sFilterConfig.FilterNumber = 0;

sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;

sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;

sFilterConfig.FilterIdHigh = 0x0000;

sFilterConfig.FilterIdLow = 0x0000;

sFilterConfig.FilterMaskIdHigh = 0x0000;

sFilterConfig.FilterMaskIdLow = 0x0000;

sFilterConfig.FilterFIFOAssignment = 0;

sFilterConfig.FilterActivation = ENABLE;

sFilterConfig.BankNumber = 14;

if (HAL_CAN_ConfigFilter(&hcan, &sFilterConfig) != HAL_OK)

{

/* Filter configuration Error */

Error_Handler();

}

}

void HAL_CAN_MspInit(CAN_HandleTypeDef* canHandle)

{

GPIO_InitTypeDef GPIO_InitStruct;

if(canHandle->Instance==CAN1)

{

/* USER CODE BEGIN CAN1_MspInit 0 */

/* USER CODE END CAN1_MspInit 0 */

/* CAN1 clock enable */

__HAL_RCC_CAN1_CLK_ENABLE();

/**CAN GPIO Configuration

PB8 ------> CAN_RX

PB9 ------> CAN_TX

*/

GPIO_InitStruct.Pin = GPIO_PIN_8;

GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

GPIO_InitStruct.Pull = GPIO_PULLUP;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

GPIO_InitStruct.Pin = GPIO_PIN_9;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

__HAL_AFIO_REMAP_CAN1_2();

/* CAN1 interrupt Init */

HAL_NVIC_SetPriority(USB_LP_CAN1_RX0_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(USB_LP_CAN1_RX0_IRQn);

/* USER CODE BEGIN CAN1_MspInit 1 */

/* USER CODE END CAN1_MspInit 1 */

}

}

void HAL_CAN_MspDeInit(CAN_HandleTypeDef* canHandle)

{

if(canHandle->Instance==CAN1)

{

/* USER CODE BEGIN CAN1_MspDeInit 0 */

/* USER CODE END CAN1_MspDeInit 0 */

/* Peripheral clock disable */

__HAL_RCC_CAN1_CLK_DISABLE();

/**CAN GPIO Configuration

PB8 ------> CAN_RX

PB9 ------> CAN_TX

*/

HAL_GPIO_DeInit(GPIOB, GPIO_PIN_8|GPIO_PIN_9);

/* CAN1 interrupt Deinit */

HAL_NVIC_DisableIRQ(USB_LP_CAN1_RX0_IRQn);

/* USER CODE BEGIN CAN1_MspDeInit 1 */

/* USER CODE END CAN1_MspDeInit 1 */

}

}

/* USER CODE BEGIN 1 */

u8 Can_Send_Msg(u8 i,u8* msg,u8 len)

{

u8 j=0;

switch(i)

{

case 0:TxMessage.StdId = 0x200;break;

case 1:TxMessage.StdId = 0x1FF;break;

}

TxMessage.IDE=CAN_ID_STD; // ???

TxMessage.RTR=CAN_RTR_DATA; // ???

TxMessage.DLC=len; // ????????

for(j=0;j<len;j++)

TxMessage.Data[j]=msg[j];

if (HAL_CAN_Transmit(&hcan, 10) != HAL_OK)

{

/* Transmition Error */

Error_Handler();

}

return 1;

}

u8 Can_Receive_Msg(u8 *buf)

{

u32 i;

if((RxMessage.StdId|0x0F)==0x20F)

{

for(i=0;i<RxMessage.DLC;i++) buf[i] = RxMessage.Data[i];

buf[7] = RxMessage.StdId - 0x201;

return RxMessage.DLC;

}

else return 0;

}

/***************RX????************/

void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* hcan)

{

if (HAL_CAN_Receive_IT(hcan, CAN_FIFO0) != HAL_OK)

{

/* Reception Error */

Error_Handler();

}

Can_Receive_Msg(RxMessage.Data);

}

/* USER CODE END 1 */

#can-hal_can_transmit_it #bug? #stm32f1-hal
This topic has been closed for replies.
Wei RP
Wei RPBest answer
Associate
Jun 15, 2018 1:27 PM UTC
Posted on June 15, 2018 at 15:27

I solved the problem.

it's a stupid reason.  I set a wrong BITRATE of the CAN BUS of controller...

3 replies

T J
Senior III
Jun 15, 2018 10:05 AM UTC
Posted on June 15, 2018 at 12:05

are you running a line driver  ?

do you have at least two devices on the network ?

do you have a terminator on the bus ?

Wei RP
Wei RPAuthor
Associate
Jun 15, 2018 2:23 PM UTC
Posted on June 15, 2018 at 14:23

thank you for your reply. i use it to run a DC motor with speed controller.

i succeed by using StdPeriph_Lib ,but failed by HAL with CubeMX. So i think my hardware should be OK.

So, is there any other possible factor will cause 

HAL_CAN_Transmit() Time out?

thx again for ur reply!

Wei RP
Wei RPAuthorBest answer
Associate
Jun 15, 2018 1:27 PM UTC
Posted on June 15, 2018 at 15:27

I solved the problem.

it's a stupid reason.  I set a wrong BITRATE of the CAN BUS of controller...