Skip to main content
zyimi
Associate
Jul 28, 2025 1:09 AM UTC
Question

The F429 uses both SDRAM and SRAM

Whether the two buses can be used at the same time? Winbond's SDRAM is used to find a high probability of reading and writing errors in SDRAM data。 but there is no problem with using ISSI. If you don't read or write to the external SRAM, it's fine。

This topic has been closed for replies.

1 reply

TDK
Jul 28, 2025 1:18 AM UTC

Yes, SRAM and SDRAM can be used at the same time. Try slowing the SDRAM clock rate down by a factor of 10, could be a layout or noise issue.

"If you feel a post has answered your question, please click ""Accept as Solution""."