Skip to main content
SP.7
Visitor II
October 4, 2021
Question

The DMA buffer configured with a multichannel ADC setup ( Processor STM32f769II) shows values in different buffer location with respect to the rank configured in the ADC setup. How can this be fixed?

  • October 4, 2021
  • 0 replies
  • 456 views

We have connected 7 channels in ADC2 to a STM32F769II processor. The DMA to ADC is enabled and the rank for conversion too is configured. But on testing, the ADC values are being shown in buffer location very different from its rank.

This happened in debug mode. But when turned off optimization, those values are shown as per the rank of the ADC channels. The DMA buffer acts differently to different compilation configurations, and to different optimizations.

This topic has been closed for replies.