Skip to main content
Associate
Jul 10, 2025 7:47 AM UTC
Question

The consumption of Vcap about the STM32H723

Hi ST expert

I'm ready to use STM32H723 now. Vcores can use internal LDOs or external power supplies via Vcap pins. If you use an external power supply, what is the current of the power supply, I see that there is only Idd in the datasheet.

Thanks

This topic has been closed for replies.

1 reply

ST Employee
Aug 5, 2025 2:28 PM UTC

Hello @licunxu, 

The current consumption can be estimated based on the datasheet values for LDO mode. For example:

  • At VOS0 (1.36V), the current consumption is approximately 145mA, resulting in a power consumption of 197mW (1.36V x 145mA).
  • Considering an 80% SMPS efficiency for example, the input power to the SMPS would be around 236.4mW, leading to an input current of approximately 71.6mA at 3.3V.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.