Skip to main content
wquan
Visitor II
November 29, 2018
Question

The chip is STM32L486VGT6. I can use the usart wake up the stop1 mode,but I can not wake up with the irda(usart3) mode .Please help!!!

  • November 29, 2018
  • 0 replies
  • 521 views

The chip is STM32L486VGT6. I can use the usart wake up the stop1 mode,but I can not wake up with the irda(usart3) mode .Please help!!!

#define UartHandle hirda3
void Stop_IRDA(void)
{
	UART_WakeUpTypeDef WakeUpSelection;
	/* make sure that no UART transfer is on-going */ 
 while(__HAL_UART_GET_FLAG(&UartHandle, USART_ISR_BUSY) == SET);
 /* make sure that UART is ready to receive
 * (test carried out again later in HAL_UARTEx_StopModeWakeUpSourceConfig) */
 while(__HAL_UART_GET_FLAG(&UartHandle, USART_ISR_REACK) == RESET);
 
 /* set the wake-up event:
 * specify wake-up on RXNE flag */
 WakeUpSelection.WakeUpEvent = UART_WAKEUP_ON_READDATA_NONEMPTY;
 if (HAL_IRDAEx_StopModeWakeUpSourceConfig(&UartHandle, WakeUpSelection)!= HAL_OK)
 {
 LED3_ON;
 }
 
 /* Enable the UART Wake UP from STOP1 mode Interrupt */
 __HAL_UART_ENABLE_IT(&UartHandle, UART_IT_WUF);
 
 /* enable MCU wake-up by UART */
 HAL_IRDAEx_EnableStopMode(&UartHandle);
 
	printf("CR1:0x%08X\r\n",UartHandle.Instance->CR1);
	printf("CR2:0x%08X\r\n",UartHandle.Instance->CR2);
	printf("CR3:0x%08X\r\n",UartHandle.Instance->CR3);
	printf("enter STOP1 mode");
 /* enter STOP1 mode */
 HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);
	for(uint8_t i = 0; i<10;i++)
	{
		LED1_TOG;
		HAL_Delay(50);
	}
 /* at that point, MCU has been awoken: the LED has been turned back on */
 SystemClock_Config();
	HAL_IRDAEx_DisableStopMode(&UartHandle);
}
 
 
 
 
 
/**
 * @brief Initialize the IRDA wake-up from stop mode parameters when triggered by address detection.
 * @param hirda IRDA handle.
 * @param WakeUpSelection IRDA wake up from stop mode parameters.
 * @retval None
 */
static void IRDAEx_Wakeup_AddressConfig(IRDA_HandleTypeDef *hirda, UART_WakeUpTypeDef WakeUpSelection)
{
 assert_param(IS_UART_ADDRESSLENGTH_DETECT(WakeUpSelection.AddressLength));
 
 /* Set the USART address length */
 MODIFY_REG(hirda->Instance->CR2, USART_CR2_ADDM7, WakeUpSelection.AddressLength);
 
 /* Set the USART address node */
 MODIFY_REG(hirda->Instance->CR2, USART_CR2_ADD, ((uint32_t)WakeUpSelection.Address << UART_CR2_ADDRESS_LSB_POS));
}
 
/**
 * @brief Handle IRDA Communication Timeout.
 * @param hirda Pointer to a IRDA_HandleTypeDef structure that contains
 * the configuration information for the specified IRDA module.
 * @param Flag Specifies the IRDA flag to check.
 * @param Status Flag status (SET or RESET)
 * @param Tickstart Tick start value
 * @param Timeout Timeout duration
 * @retval HAL status
 */
static HAL_StatusTypeDef __IRDA_WaitOnFlagUntilTimeout(IRDA_HandleTypeDef *hirda, uint32_t Flag, FlagStatus Status, uint32_t Tickstart, uint32_t Timeout)
{
 /* Wait until flag is set */
 while ((__HAL_IRDA_GET_FLAG(hirda, Flag) ? SET : RESET) == Status)
 {
 /* Check for the Timeout */
 if (Timeout != HAL_MAX_DELAY)
 {
 if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U))
 {
 /* Disable TXE, RXNE, PE and ERR (Frame error, noise error, overrun error) interrupts for the interrupt process */
#if defined(USART_CR1_FIFOEN)
 CLEAR_BIT(hirda->Instance->CR1, (USART_CR1_RXNEIE_RXFNEIE | USART_CR1_PEIE | USART_CR1_TXEIE_TXFNFIE));
#else
 CLEAR_BIT(hirda->Instance->CR1, (USART_CR1_RXNEIE | USART_CR1_PEIE | USART_CR1_TXEIE));
#endif
 CLEAR_BIT(hirda->Instance->CR3, USART_CR3_EIE);
 
 hirda->gState = HAL_IRDA_STATE_READY;
 hirda->RxState = HAL_IRDA_STATE_READY;
 
 /* Process Unlocked */
 __HAL_UNLOCK(hirda);
 return HAL_TIMEOUT;
 }
 }
 }
 return HAL_OK;
}
 
/**
 * @brief Set Wakeup from Stop mode interrupt flag selection.
 * @note It is the application responsibility to enable the interrupt used as
 * usart_wkup interrupt source before entering low-power mode.
 * @param hirda IRDA handle.
 * @param WakeUpSelection Address match, Start Bit detection or RXNE/RXFNE bit status.
 * This parameter can be one of the following values:
 * @arg @ref IRDA_WAKEUP_ON_ADDRESS
 * @arg @ref IRDA_WAKEUP_ON_STARTBIT
 * @arg @ref IRDA_WAKEUP_ON_READDATA_NONEMPTY
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_IRDAEx_StopModeWakeUpSourceConfig(IRDA_HandleTypeDef *hirda, UART_WakeUpTypeDef WakeUpSelection)
{
 HAL_StatusTypeDef status = HAL_OK;
 uint32_t tickstart = 0U;
 
 /* check the wake-up from stop mode IRDA instance */
 assert_param(IS_UART_WAKEUP_FROMSTOP_INSTANCE(hirda->Instance));
 /* check the wake-up selection parameter */
 assert_param(IS_UART_WAKEUP_SELECTION(WakeUpSelection.WakeUpEvent));
 
 /* Process Locked */
 __HAL_LOCK(hirda);
 
 hirda->gState = HAL_IRDA_STATE_BUSY;
 
 /* Disable the Peripheral */
 __HAL_IRDA_DISABLE(hirda);
 
 /* Set the wake-up selection scheme */
 MODIFY_REG(hirda->Instance->CR3, USART_CR3_WUS, WakeUpSelection.WakeUpEvent);
 
 if (WakeUpSelection.WakeUpEvent == UART_WAKEUP_ON_ADDRESS)
 {
 IRDAEx_Wakeup_AddressConfig(hirda, WakeUpSelection);
 }
 
 /* Enable the Peripheral */
 __HAL_IRDA_ENABLE(hirda);
 
 /* Init tickstart for timeout managment*/
 tickstart = HAL_GetTick();
 
 /* Wait until REACK flag is set */
 if (__IRDA_WaitOnFlagUntilTimeout(hirda, USART_ISR_REACK, RESET, tickstart, HAL_UART_TIMEOUT_VALUE) != HAL_OK)
 {
 status = HAL_TIMEOUT;
 }
 else
 {
 /* Initialize the IRDA State */
 hirda->gState = HAL_IRDA_STATE_READY;
 }
 
 /* Process Unlocked */
 __HAL_UNLOCK(hirda);
 
 return status;
}
/**
 * @brief Enable IRDA Stop Mode.
 * @note The IRDA is able to wake up the MCU from Stop 1 mode as long as IRDA clock is HSI or LSE.
 * @param hirda IRDA handle.
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_IRDAEx_EnableStopMode(IRDA_HandleTypeDef *hirda)
{
 /* Process Locked */
 __HAL_LOCK(hirda);
 
 /* Set UESM bit */
 SET_BIT(hirda->Instance->CR1, USART_CR1_UESM);
 
 /* Process Unlocked */
 __HAL_UNLOCK(hirda);
 
 return HAL_OK;
}
 
/**
 * @brief Disable IRDA Stop Mode.
 * @param hirda IRDA handle.
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_IRDAEx_DisableStopMode(IRDA_HandleTypeDef *hirda)
{
 /* Process Locked */
 __HAL_LOCK(hirda);
 
 /* Clear UESM bit */
 CLEAR_BIT(hirda->Instance->CR1, USART_CR1_UESM);
 
 /* Process Unlocked */
 __HAL_UNLOCK(hirda);
 
 return HAL_OK;
}
 
void SystemClock_Config(void)
{
 
 RCC_OscInitTypeDef RCC_OscInitStruct;
 RCC_ClkInitTypeDef RCC_ClkInitStruct;
 RCC_PeriphCLKInitTypeDef PeriphClkInit;
 
 /**Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 5;
 RCC_OscInitStruct.PLL.PLLN = 32;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART2
 |RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_UART4
 |RCC_PERIPHCLK_LPUART1|RCC_PERIPHCLK_I2C2
 |RCC_PERIPHCLK_SDMMC1;
 PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
 PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
 PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_HSI;
 PeriphClkInit.Uart4ClockSelection = RCC_UART4CLKSOURCE_PCLK1;
 PeriphClkInit.Lpuart1ClockSelection = RCC_LPUART1CLKSOURCE_PCLK1;
 PeriphClkInit.I2c2ClockSelection = RCC_I2C2CLKSOURCE_PCLK1;
 PeriphClkInit.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_PLLSAI1;
 PeriphClkInit.PLLSAI1.PLLSAI1Source = RCC_PLLSOURCE_HSE;
 PeriphClkInit.PLLSAI1.PLLSAI1M = 5;
 PeriphClkInit.PLLSAI1.PLLSAI1N = 16;
 PeriphClkInit.PLLSAI1.PLLSAI1P = RCC_PLLP_DIV7;
 PeriphClkInit.PLLSAI1.PLLSAI1Q = RCC_PLLQ_DIV2;
 PeriphClkInit.PLLSAI1.PLLSAI1R = RCC_PLLR_DIV2;
 PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_48M2CLK;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Configure the main internal regulator output voltage 
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
 
 /**Configure the Systick interrupt time 
 */
 HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
 /**Configure the Systick 
 */
 HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
 /* SysTick_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}

    This topic has been closed for replies.