Skip to main content
SAbis
Associate II
December 10, 2018
Question

The µC STM32F051Kx has only one SPI and of course only one CS (chip select). It is possiblie to use another and configure it as CS?

..

This topic has been closed for replies.

2 replies

Uwe Bonnes
Chief
December 10, 2018

Of course you can bitbang other pins as CS.

SAbis
SAbisAuthor
Associate II
December 10, 2018

thanks very much.

do you have any idea on using the UART interface to upload Firmware? We are using only this interface to communicate between our controller and to reduce the Pin-number and an extra connector for SWD (serial wired debu), I am planning directly to use the same communication interface (RS485) to upload my firmware. is this possible? if yes how could i realise it in Hardware?

Thanks