Question
Terminal treatment of the STM32F479BIT6 when the MIPI circuit is not used
Questions about STM32F479BIT6
If the MIPI circuit is unused and
The following pins are NC,pull-up,pull-down
Which terminal treatment should I use?
Target Terminals
119/120/121/122/122/122/124/124/125/126/127/128/