Skip to main content
camille
Associate II
December 27, 2011
Question

Temperature sensor on ADC2

  • December 27, 2011
  • 2 replies
  • 754 views
Posted on December 27, 2011 at 17:34

Hi everybody.

I've just a little question : does anyone knows if the internal temperature sensor of an STM32F107 can be read with ADC2. In the reference manual it's written ''The temperature sensor is internally connected to the ADCx_IN16 input channel'' but on figure 39 Vsense and Vref are clearly connected to ADC1.

However I'm trying to use ADC2 to read internal temperature sensor value but I just get very very low values (0x01...0x07) while with ADC1 values are Ok.

Thanks a lot.

Robin.
    This topic has been closed for replies.

    2 replies

    raptorhal2
    Lead
    December 28, 2011
    Posted on December 28, 2011 at 16:06

    Other sections in the reference manual are more specific. RM0008 Rev 13 Section 11.3.3 says:

    ''Note: The sensor and VREFINT are only available on the master ADC1 peripheral.''

    Figure 29 shows the temp sensor and VRef going to ADC1, but only IN_0 to IN_15 go to ADC2.

    Cheers, Hal

    camille
    camilleAuthor
    Associate II
    December 28, 2011
    Posted on December 28, 2011 at 21:55

    Ok thank you very much. Next time i'll read more carefully all the paragraph ;)

    Regards.

    Robin