Skip to main content
kapilsinghi123
Associate II
June 23, 2017
Question

TCP/IP Server and Client on one device?

  • June 23, 2017
  • 0 replies
  • 384 views
Posted on June 23, 2017 at 10:01

Hello All,

I tried to run client and server in two different threads with two different ports (server with port 80 and client with 1234)

But the moment my client attached to the respective server on Internet, Local Server application stops responding !!

I am using the netcom example provided in Cube2 ,

Device used is F207 and compiling code in Keil.

Need help !

    This topic has been closed for replies.